Skip to main content
Vikram baliga
Associate II
February 28, 2018
Solved

H3LIS331DL: Acceleration is shown in all the 3 axis. Not just the axis in which I had hit it.

  • February 28, 2018
  • 3 replies
  • 1271 views
Posted on February 28, 2018 at 05:30

If i shake the sensor board, acceleration is produced in the corresponding axis. but if i tap on the board, to produce higher g values, say 200g - 400g, the acceleration spike is seen in all the 3 axis, not just axis which I had tapped.

#h3lis331dl #h3lis331dl-working
This topic has been closed for replies.
Best answer by Miroslav BATEK
Posted on April 19, 2018 at 10:08

The configuration seems to be correct and the behavior is normal. The tap is never be exactly along one axis so the sensor will move little bit in all directions.

3 replies

ST Employee
February 28, 2018
Posted on February 28, 2018 at 09:26

Please provide your sensor configuration and a plot of X, Y, Z data during the tap.

Vikram baliga
Associate II
April 17, 2018
Posted on April 17, 2018 at 11:08

Configuration data sent via I2C in the following order:  

                                                            Register address   Value written

Set data rate and enable all 3 axis :            0x20                   0x3F

Scale selection : +/- 400g :                          0x23                   0x30

Filter settings for offsetting the errors :        0x21                   0x1F

Reference for high pass filter = 0g :            0x26                   0x00

Interrupt threshold :                                     0x32                   0x70

 

Interrupt setting :                                         0x30                   0x2A

Plot of all the 3 axes during tap:

Data rate 1 kHz. 

0690X0000060AciQAE.png
Miroslav BATEKBest answer
ST Employee
April 19, 2018
Posted on April 19, 2018 at 10:08

The configuration seems to be correct and the behavior is normal. The tap is never be exactly along one axis so the sensor will move little bit in all directions.