Skip to main content
Bhavan Raibagi
Associate
May 19, 2017
Question

STM8AF52AATCY

  • May 19, 2017
  • 1 reply
  • 734 views
Posted on May 19, 2017 at 13:21

Dear Sir/Madam,

How to make controller goes into sleep mode. Can you please give me information or send me any source code link. Here, I am making into sleep using halt(); mode with disabling the peripherals but I'm thinking that Is there any other configuration need to do. Kindly, suggest me to solve this issue.

    This topic has been closed for replies.

    1 reply

    Bhavan Raibagi
    Associate
    May 23, 2017
    Posted on May 23, 2017 at 13:35

    Dear Sir/Madam,

    Now I did controller into halt completely. But when it's in halt mode if any GPIO external interrupt is triggered means it wakes up, but when I will send the CAN Identifier then It's not waking up. As per data sheet in halt mode if CAN_RX interrupt comes it should wake up. So, can you please guide to me what initialization I need configure for CAN before entering into the halt mode. Here I added CAN_Config(); function.

    void CAN_Config(void)

    {

    CAN_InitStatus_TypeDef status = CAN_InitStatus_Failed;

    /* Filter Parameters */

    CAN_FilterNumber_TypeDef CAN_FilterNumber;

    FunctionalState CAN_FilterActivation;

    CAN_FilterMode_TypeDef CAN_FilterMode;

    CAN_FilterScale_TypeDef CAN_FilterScale;

    uint8_t CAN_FilterID1;

    uint8_t CAN_FilterID2;

    uint8_t CAN_FilterID3;

    uint8_t CAN_FilterID4;

    uint8_t CAN_FilterIDMask1;

    uint8_t CAN_FilterIDMask2;

    uint8_t CAN_FilterIDMask3;

    uint8_t CAN_FilterIDMask4;

    /* Init Parameters*/

    CAN_MasterCtrl_TypeDef CAN_MasterCtrl;

    CAN_Mode_TypeDef CAN_Mode;

    CAN_SynJumpWidth_TypeDef CAN_SynJumpWidth;

    CAN_BitSeg1_TypeDef CAN_BitSeg1;

    CAN_BitSeg2_TypeDef CAN_BitSeg2;

    uint8_t CAN_Prescaler;

    /* CAN register init */

    CAN_DeInit();

    /* CAN init */

    CAN_MasterCtrl=CAN_MasterCtrl_AllEnabled;

    //CAN Loop Back Mode JNa

    //CAN_Mode = CAN_Mode_LoopBack;

    CAN_Mode = CAN_Mode_Normal;

    /*CAN_SynJumpWidth = CAN_SynJumpWidth_1TimeQuantum;

    CAN_BitSeg1 = CAN_BitSeg1_5TimeQuantum;

    CAN_BitSeg2 = CAN_BitSeg2_2TimeQuantum;

    CAN_Prescaler = 4;*/

    CAN_SynJumpWidth = CAN_SynJumpWidth_1TimeQuantum;

    CAN_BitSeg1 = CAN_BitSeg1_8TimeQuantum;

    CAN_BitSeg2 = CAN_BitSeg2_7TimeQuantum;

    CAN_Prescaler = 8; /* 500kbit/s */

    status = CAN_Init(CAN_MasterCtrl, CAN_Mode, CAN_SynJumpWidth, CAN_BitSeg1, \

    CAN_BitSeg2, CAN_Prescaler);

    /* CAN filter init */

    CAN_FilterNumber = CAN_FilterNumber_0;

    CAN_FilterActivation = ENABLE;

    CAN_FilterMode = CAN_FilterMode_IdMask;

    CAN_FilterScale = CAN_FilterScale_32Bit;

    CAN_FilterID1=0;

    CAN_FilterID2=0;

    CAN_FilterID3=0;

    CAN_FilterID4=0;

    CAN_FilterIDMask1=0;

    CAN_FilterIDMask2=0;

    CAN_FilterIDMask3=0;

    CAN_FilterIDMask4=0;

    CAN_FilterInit(CAN_FilterNumber, CAN_FilterActivation, CAN_FilterMode,

    CAN_FilterScale,CAN_FilterID1, CAN_FilterID2, CAN_FilterID3,

    CAN_FilterID4,CAN_FilterIDMask1, CAN_FilterIDMask2,

    CAN_FilterIDMask3, CAN_FilterIDMask4);

    /* Enable Fifo message pending interrupt*/

    /* Message reception is done by CAN_RX ISR*/

    CAN_ITConfig(CAN_IT_FMP, ENABLE);

    }

    Here, I am suspecting about my configuration, what configuration need to be change.