STM32CubeMX generate incomplete code for an LL based STM32L1 project
- September 9, 2017
- 21 replies
- 5791 views
Update:
As the below error appeared when I tried to make a Low Layer project for Nucleo L152RE board using STM32CubeMX in generating a code for a Makefile project, and, it was solved by an update to both STM32CubeMX and LL driver, the generated code remains unusable so, I chose a more appropriate title.
Original topic:
- undefined reference to `LL_RCC_GetSystemClocksFreq'
This function is referenced inside LL_I2C_Init function. I am using the last version of STM32CubeMX and I'm writing code for Nucleo L152RE board using Low Layer drivers.
I generated code for using the I2C1 peripheral, and I did a compilation without adding my own code. And it trows the error specified in the title at linker time. I also use the last version of ARM gcc compiler from the gcc-arm-none-eabi-6-2017-q2-update-linux.tar.bz2 archive under Linux Fedora 26.
I attached the project archive.
#stm32cubemx #i2c #timer #incomplete-code #undeleted-temporary-files #missing-files #beta-quality #nucleo-l152re #linker-error