Why does STM32F4 Discovery kit
Hi,
I've just got a STM32F4 Discovery kit (STM32F429)
I thought that it embedded software for demonstate at the first time.
But my kit does not work.I also I read the below instruction.
But I don't know should I have to re-fund this kit?
What am I missing?
Getting started Follow the sequence below to configure the STM32F429 Discovery board and launch the DISCOVER application: 1. Ensure that the jumpers JP3 and CN4 are set to 'ON' (Discovery mode). 2. Connect the STM32F429 Discovery board to a PC using a USB cable type A/mini-B through the USB ST-LINK connector CN1, to power the board, the LEDs LD2 (PWR) and LD1 (COM). 3. The following applications are available on the screen: – Clock/Calendar and Game – Video Player and Image Browser (play videos and view images from the USB mass storage connected to CN6) – Performance monitor (watch the CPU load and run a graphical benchmark) – System Info 4. The demo software, as well as other software examples are available at the www.st.com/stm32f4-discovery webpage. 5. Develop applications starting from the examples.