Question
sprintf function does not work in keil compiler
Posted on September 15, 2017 at 22:38
Hi to all
I am new in STM32 and keil (I used Atmel chips) and now I am getting familier with them.
I made a project and I can send data to serial port with the following function :
'HAL_UART_Transmit(&huart1,(uint8_t *) 'Hello\n\r', 7, 10);'
but I do not know why there is no data when I use the following function based on sprintf:
'sprintf((char *) buffer,'23');'
The thing is that the code is well compiled and there is no error but the function does not work.
Do I need to add some more code for sprintf function ??!!!
Help please
:)