Skip to main content
Ali Rezaei
Associate
September 15, 2017
Question

sprintf function does not work in keil compiler

  • September 15, 2017
  • 4 replies
  • 2860 views
Posted on September 15, 2017 at 22:38

Hi to all

I am new in STM32 and keil (I used Atmel chips) and now I am getting familier with them.

I made a project and I can send data to serial port with the following function :

'HAL_UART_Transmit(&huart1,(uint8_t *) 'Hello\n\r', 7, 10);'

but I do not know why there is no data when I use the following function based on sprintf:

'sprintf((char *) buffer,'23');'

The thing is that the code is well compiled and there is no error but the function does not work.

Do I need to add some more code for sprintf function ??!!!

Help please  

:)

    This topic has been closed for replies.

    4 replies

    Tesla DeLorean
    Guru
    September 18, 2017
    Posted on September 18, 2017 at 11:53

    sprintf creates data in the buffer not output to the console.  Show more complete example.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    Tilen MAJERLE
    ST Employee
    September 18, 2017
    Posted on September 18, 2017 at 12:02

    When using sprintf function, you must declare buffer where sprint function will format output string and then you can send it via UART.

    Something similar to:

    char buffer[10];
    sprintf(buffer, 'Hello
    
    ');
    HAL_UART_Transmit(&huart, (uint8_t *)buffer, strlen(buffer), 100);�?�?�?�?

    If you want to output data directly, then take a look at printf and not sprintf. In this case, you will have to implement fputc callback function.

    Best regards,

    Tilen

    Ali Rezaei
    Associate
    September 18, 2017
    Posted on September 18, 2017 at 16:00

     ,

     ,

    Hi

    thanks for your help. here is my simple code with works with sprintf function as you explained but still have a problem with printf

    function

    . I guess I did something wrong in fputc callback

    function

    . Do you have any idea? ,

    it is a simple code. it waits until a push button pressed, then it turns on a LED and sends 3 data to PC console with 3 different

    function

    .

    1- MCU transmit

    function

    .

    2- filling a string and sending with MCU transmit

    function

    .

    3- with printf

    function

    .

    it is just to check how different

    functions

    work in STM32F0 and keil.

    it works but instead of having value 23 with printf function, I have two Small square on screen.

    /* Includes ------------------------------------------------------------------*/

     ,

    ♯ include 'main.h'

     ,

    ♯ include 'stm32f0xx_hal.h'

     ,

    ♯ include 'stdio.h'

    /* USER CODE BEGIN Includes */

    /* USER CODE END Includes */

    /* Private variables ---------------------------------------------------------*/

     ,

    UART_HandleTypeDef huart1,

    /* USER CODE BEGIN PV */

     ,

    /* Private variables ---------------------------------------------------------*/

    char buffer[20],

     ,

    char a[1] = 'A',

    /* USER CODE END PV */

    /* Private function prototypes -----------------------------------------------*/

     ,

    void SystemClock_Config(void),

     ,

    static void MX_GPIO_Init(void),

     ,

    static void MX_USART1_UART_Init(void),

    /* USER CODE BEGIN PFP */

     ,

    /* Private function prototypes -----------------------------------------------*/

     ,

    /* USER CODE END PFP */

     ,

    /* USER CODE BEGIN 0 */

    struct __FILE {int hndle,},

     ,

    FILE __stdout,

     ,

    FILE __stdin,

     ,

    FILE __stderr,

     ,

    int fputc(int ch, FILE *f)

     ,

    {

     ,

    while (!HAL_UART_GetState(&,huart1)),

     ,

    HAL_UART_Transmit(&,huart1,(uint8_t *) ch, 20,100),

     ,

    return ch,

     ,

    }

    /* USER CODE END 0 */

    int main(void)

     ,

    {

    /* USER CODE BEGIN 1 */

    /* USER CODE END 1 */

    /* MCU Configuration----------------------------------------------------------*/

    /* Reset of all peripherals, Initializes the Flash interface and the Systick. */

     ,

    HAL_Init(),

    /* USER CODE BEGIN Init */

    /* USER CODE END Init */

    /* Configure the system clock */

     ,

    SystemClock_Config(),

    /* USER CODE BEGIN SysInit */

    /* USER CODE END SysInit */

    /* Initialize all configured peripherals */

     ,

    MX_GPIO_Init(),

     ,

    MX_USART1_UART_Init(),

    /* USER CODE BEGIN 2 */

     ,

    HAL_UART_Transmit(&,huart1,(uint8_t *) 'Hello', 5, 10),

    /* USER CODE END 2 */

    /* Infinite loop */

     ,

    /* USER CODE BEGIN WHILE */

     ,

    while (1)

     ,

    {

     ,

    /* USER CODE END WHILE */

    /* USER CODE BEGIN 3 */

     ,

    if (HAL_GPIO_ReadPin (GPIOA,GPIO_PIN_0) == 1){

     ,

    HAL_GPIO_WritePin(GPIOC,LD3_Pin,GPIO_PIN_SET),

     ,

    HAL_UART_Transmit(&,huart1,(uint8_t *) 'Hello\n\r', 7, 10),

     ,

    sprintf(buffer,'hello world'),

     ,

    HAL_UART_Transmit(&,huart1,(uint8_t *) buffer, 20, 10),

     ,

    printf('23'),

     ,

    HAL_Delay(300),

     ,

    }

     ,

    else if (HAL_GPIO_ReadPin(GPIOA,GPIO_PIN_0) == 0){

     ,

    HAL_GPIO_WritePin(GPIOC,LD3_Pin,GPIO_PIN_RESET),

     ,

    }

     ,

     ,

    }

     ,

    /* USER CODE END 3 */

    }

    Tesla DeLorean
    Guru
    September 18, 2017
    Posted on September 18, 2017 at 16:59

    HAL_UART_Transmit(&huart1,(uint8_t *) ch, 20,100); // NO NOT LIKE THIS

    HAL_UART_Transmit(&huart1,(uint8_t *) &ch, 1,100); // You need a POINTER to the variable and sending ONE character

    HAL_UART_Transmit(&huart1,(uint8_t *) buffer, strlen(buffer), 100); // Get the length right, the timeout long enough

    //******************************************************************************

    // Hosting of stdio functionality through USART1

    //******************************************************************************

    void outchar(int x)

    {

      while((USART1->ISR & USART_ISR_TXE) == 0);

      USART1->TDR = x;

    }

    //******************************************************************************

    int inchar(void)

    {

      while((USART1->ISR & USART_ISR_RXNE) == 0);

      return((int)USART1->RDR & 0xFF);

    }

    //******************************************************************************

    #include <rt_misc.h>

    #pragma import(__use_no_semihosting_swi)

    struct __FILE { int handle; /* Add whatever you need here */ };

    FILE __stdout;

    FILE __stdin;

    int fputc(int ch, FILE *f)

    {

      outchar(ch);

      return(ch);

    }

    int fgetc(FILE *f)

    {

      return(inchar());

    }

    int ferror(FILE *f)

    {

      /* Your implementation of ferror */

      return EOF;

    }

    void _ttywrch(int ch)

    {

      outchar(ch);

    }

    void _sys_exit(int return_code)

    {

    label:  goto label;  /* endless loop */

    }

    //******************************************************************************

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..