ADC /DMA Problem STM32F100
ADC1 converts every 500us 5 analog channels ( ADC10/11/12/13/14) and write the result via DMA1 to internal SRAM (ADResult[5]) in this order [ ADC10,ADC11,ADC12,ADC13,ADC14]. This works fine, but randomly after some houres or days the result order in memory is corrupted to [ADC14,ADC10,ADC11,ADC12,ADC13], shift at one Position and stay in this wrong order all the time.
ADC1 is configured in Scan Mode, not continuous conversion:
// ADC Konfiguration (regular group = ADC10/11/12/13/14
RCC->APB2ENR|=RCC_APB2ENR_ADC1EN; //enable Clock for ADC1 ADC1->SQR1=0x00400000; //5 Kanäle ADC1->SMPR1=0x00ffffff; ADC1->SMPR2=0x3fffffff; //Abstastzeit der Kanäle auf 240 Zyklen ADC1->SQR3=0x1ee6b16a; //Abtastreihenfolge festlegen 10/11/12/13/14 ADC1->CR1=0x00000100; //use independant mode, SCAN mode ADC1->CR2=0x000e0100; //use data align right,not continuous conversion // EXTSEL = SWSTARTDMA1 Configuration:
// DMA-Konfiguration für A/D-Wandler
RCC->AHBENR|=RCC_AHBENR_DMA1EN; // enable Clock for DMA1 DMA1_Channel1->CMAR=(u32)ADValue; // DMA-Zieladresse setzen DMA1_Channel1->CPAR=(u32)&(ADC1->DR); // DMA-Quelladresse setzen DMA1_Channel1->CNDTR=5; // transmit 5 words DMA1_Channel1->CCR=0x00003580; // DMA konfig. (0x00000580) DMA1_Channel1->CCR|=DMA_CCR1_EN; // DMA Channel 1 enableThe ADC conversion is started in the TIM2_IRQHandler(), which is called every 500us:
void TIM2_IRQHandler(void)
{ .......
.........
TEST_PIN3(1);
ADC1->SR&=~ADC_SR_EOC; // Interrupt-Flag clear ADC1->CR2 |= 0x00500000; // start A/D conversion (0x00500000) ADC1->CR1|=ADC_CR1_EOCIE; // EOC-Interrupt enable TEST_PIN3(0);.....
.....
}After the A/D conversion of this 5 Inputs is finished ADC1_IRQHandler/() is called. Tme between start A/D conversion
and call of ADC1_IRQHandler() is 100us.
void ADC1_IRQHandler(void)
{ .........TEST_PIN3(1);
ADC1->SR&=~ADC_SR_EOC; // Interrupt-Flag löschen ADC1->CR1&=~ADC_CR1_EOCIE; // EOC-Interrupt sperren while(!(DMA1->ISR & 0x02UL)); // Warten auf Ende des DMA-Transfers DMA1->IFCR=0x02UL; // Flag löschen //DMA-Transferzähler nachladen DMA1_Channel1->CCR&=~(1<<0); // DMA Channel 1 disable DMA1_Channel1->CNDTR=5; // transmit 5 words DMA1_Channel1->CCR|=(1<<0); // DMA Channel 1 enable........
}
Has anyone encountered a same Problem ?
Please help.