Skip to main content
Julian Winpenny
Associate III
October 3, 2017
Question

What is the best way to receive uart serial data at 115k Baud in a FreeRtos based app?

  • October 3, 2017
  • 10 replies
  • 2443 views
Posted on October 03, 2017 at 19:54

MCU: STM32F765

Using FreeRtos

    This topic has been closed for replies.

    10 replies

    Julian Winpenny
    Associate III
    October 3, 2017
    Posted on October 03, 2017 at 20:07

    The data is of variable length, so fixed length DMA transfer is not suitable

    Tesla DeLorean
    Guru
    October 3, 2017
    Posted on October 03, 2017 at 21:18

    Read it into a buffer? State machine processing/parsing in the USART IRQHandler?

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    Julian Winpenny
    Associate III
    October 3, 2017
    Posted on October 03, 2017 at 21:36

    Thanks Clive, Yes, I was thinking I'll have to use receive interrupt and write to a fifo, then read it out and process in a task.

    Richard Lowe
    Senior II
    October 3, 2017
    Posted on October 03, 2017 at 20:44

    A good rule of thumb is to use SIGNALS for ISRs and have the receiving and transmissions in separatetasks.

    Here's anexample:

    void HAL_UART_TxCpltCallback(UART_HandleTypeDef *huart)
    {
     if(huart->Instance == USART3)
     {
     osSemaphoreRelease(host_tx_semHandle);
     }
    }
    
    void HAL_UART_RxCpltCallback(UART_HandleTypeDef *huart)
    {
     if(huart->Instance == USART3 )
     {
    osSignalSet( host_rx_taskHandle, HOST_RX_ISR_FLAG );
     }
    }�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?

    These are the handlers for the tasks. On the transmission, I'm using DMA, so when the UART is finished transmission the semaphore is released.

    Here are the tasks:

    void host_rx_process(void const * argument)
    {
     // Buffer to hold message
     static uint8_t rx_buffer[HOST_RX_BUFFER] = {0};
     static uint8_t index = 0;
     static bool in_frame = false;
     uint8_t tmp_char = 0;
     HAL_UART_Receive_IT( &huart3, rx_tmp_buffer, 1 );
     for(;;)
     {
    osSignalWait( HOST_RX_ISR_FLAG, osWaitForever );
    tmp_char = *( huart3.pRxBuffPtr - huart3.RxXferSize );
    // Do whatever needs to be done to the new char that just arrived
     //....
     // Be sure to set the interrupt for the next char
     if( HAL_UART_Receive_IT( &huart3, (huart3.pRxBuffPtr - huart3.RxXferSize), 1 ) != HAL_OK)
     {
     Error_Handler();
     }
     }
    }
    �?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?

    What's important here is that I'm waiting for the signal to the rx process which is set by the ISR handler. Doing this saves the most amount of cycles on the ISR so the RTOS can manage the tasks effectively.

    Julian Winpenny
    Associate III
    October 10, 2017
    Posted on October 10, 2017 at 17:58

    Thanks Richard. The receive process works well.

    How would the transmit process work please ?

    Richard Lowe
    Senior II
    October 10, 2017
    Posted on October 10, 2017 at 18:32

    Something like:

    void host_tx_process(void const * argument)
    {
    osEvent evt;
    for(;;)
    {
    evt = osMessageGet(host_tx_handle, WDT_MAX_WAIT_TIME );
    if( evt.status == osEventMessage )
    {
    message_t *msg = (message_t*)evt.value.p;
    // Take binary semaphore for UART
    osSemaphoreWait(host_tx_semHandle, osWaitForever);
    memcpy( (void*)&tx_buffer[4], (void*)msg->buffer, msg->msg_len );
    tx_buffer[msg->msg_len++] = END_OF_FRAME;
    HAL_UART_Transmit_DMA( &huart3, (uint8_t*)tx_buffer, msg->msg_len );
    osPoolFree( message_pool, msg );
    }
    }
    }�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?

    My application is specific, but the idea is passing a message to the host transmit thread and it sends everything over DMA.

    AVI-crak
    Senior
    October 3, 2017
    Posted on October 03, 2017 at 23:42

    DMA does a great job of transferring data using the FIFO buffer, and writing 32b words into memory. You need to use a communication protocol that is understandable for both sides. Even if you use your own unique data container, the required number of received or transmitted data will always be known. It came with an error in the transfer - just request the whole package again. Make it once, and use it in all your projects. Because it is a universal thing. It does not depend on the processor used, it does not depend on the compiler, it's just an algorithm - which will always be executed. Although it is much more logical to take a suitable example from an open repository, for example with GIT.

    Option when the amount of data is unknown, or just laziness.

    Use of cyclic variant of DMA operation, without checks, without detectors, without hardware capabilities of the uart block. This is a mega custom level of arduino in programming - where the contents of the memory of the receiving buffer are checked programmatically in continuous mode. Search there the same.