Question
uart with interrupt stm32L4
Posted on March 28, 2018 at 13:02
trying to set up a UART receive with interrupt so far no success code is below im using stm32l4
any suggestions would be great thanks
#include 'stm32l4xx.h'
#include 'stm32l433xx.h'char uart3_tx_data[]=' is here again';
void Init_USART3();int indexx;char usart3_rcv_buffer[20];void USART3_IRQHandler()
{ Toogle_GPIOB_Pin(9); if ((USART1->ISR & USART_ISR_RXNE) == USART_ISR_RXNE){ send_string(usart3_rcv_buffer); usart3_rcv_buffer[indexx++] = (USART3->RDR); /* Receive data, clear flag */}}int main (void)
{ RCC->APB1ENR1 |=(1<<4); //TIM6 clock enabled TIM6->PSC = 0; // f timer = fclk / 24000 => 1kHz TIM6->ARR = 0xFFf; TIM6->CR1 = TIM_CR1_CEN; RCC->AHB2ENR |= RCC_AHB2ENR_GPIOBEN; RCC->AHB2ENR |= RCC_AHB2ENR_GPIOCEN; RCC->AHB2ENR |= RCC_AHB2ENR_GPIOAEN; GPIOC ->MODER &= ~ GPIO_MODER_MODE10_0; ///set GPIO2 as alternate functions GPIOC ->MODER |= (GPIO_MODER_MODE10_1); GPIOC ->OTYPER &= ~(GPIO_OTYPER_OT_10) ; ///push pull output type for GPIOA12 GPIOC ->OSPEEDR |= (GPIO_OSPEEDER_OSPEEDR10_0); // high speed for GPPIOC12 GPIOC ->OSPEEDR |= (GPIO_OSPEEDER_OSPEEDR10_1); GPIOC ->PUPDR &= ~(GPIO_PUPDR_PUPDR10); //NO PULL UP*/ GPIOC ->MODER &= ~ GPIO_MODER_MODE11_0; ///set GPIO2 as alternate functions GPIOC ->MODER |=(GPIO_MODER_MODE11_1); GPIOC ->OTYPER &= ~(GPIO_OTYPER_OT_11); ///push pull output type for GPIOA12 GPIOC ->OSPEEDR |= (GPIO_OSPEEDER_OSPEEDR11_0); // high speed for GPPIOC12 GPIOC ->OSPEEDR |= (GPIO_OSPEEDER_OSPEEDR11_1); GPIOC ->PUPDR &= ~(GPIO_PUPDR_PUPDR11); //NO PULL UP*/ GPIOC->AFR[1] |=(1<<28); //Alternate function 7 for PC10 USART TX GPIOC->AFR[1] |=(1<<29); GPIOC->AFR[1] |=(1<<30); GPIOC->AFR[1] &=~(1<<31); GPIOC->AFR[1] |=(1<<28); //Alternate function 7 for PC11 USART RX GPIOC->AFR[1] |=(1<<29); GPIOC->AFR[1] |=(1<<30); GPIOC->AFR[1] &=~(1<<31); Config_Lcd (); Set_GPIOB_OutPut_No_Pu(9); RCC->APB1ENR1 |= RCC_APB1ENR1_USART3EN; //enable USART3 clock USART3->BRR =4000000/96; //baud rate = 9600 USART3->CR1&=~(1<<28); //1 Start bit, 8 data bits, n stop bits USART3->CR1&=~(1<<12); USART3->CR1 |= USART_CR1_UE; // USART3 enable. USART3->CR1 |= (1<<3); // USART3 tx enable. USART3->CR2 &= ~(1<<12); //1 stop bit USART3->CR2 &= ~(1<<13); //1 stop bit // USART3->CR1 = USART_CR1_RXNEIE | USART_CR1_RE | USART_CR1_UE; char my_str[]='fooo'; __enable_irq(); //enable interrupt NVIC_SetPriority(USART3_IRQn,4); //Set priority NVIC_ClearPendingIRQ(USART3_IRQn); //clear pending NVIC_EnableIRQ(USART3_IRQn); while(1) { send_string(my_str); /* Will inititiate TC if TXE is set*/ USART3->RDR='a'; Delay_ms(1000); Clear_Lcd(); Delay_ms(1000); } return 0; }