2017-06-27 6:19 PM
Dear all
Useing CAN1 of STM32F205, 32-bit Mask Mode filter, filter bank 0-13 work all right for now.
Then I am trying to configurate CAN2SB = 28d, for letting CAN1 use all 28 filter banks.But it doesn't work, here is my part of code, would you please help me?
Thx inadvance
void can_Init(void)
{UCHAR i;RCC->APB1ENR |= RCC_APB1ENR_CAN1EN; // Enable clock for CAN
RCC->APB1RSTR |= RCC_APB1RSTR_CAN1RST; // Reset CAN module
RCC->APB1RSTR &= ~RCC_APB1RSTR_CAN1RST; // Deactivate reset
CAN1->MCR = CAN_MCR_ABOM | CAN_MCR_INRQ; // Automatic bus-off managment, init request
CAN1->IER = CAN_IER_FMPIE0 | CAN_IER_FMPIE1; // Active interrupts CAN1->BTR = ( ((CAN_1tq) << 24) | ((CAN_4tq) << 20) | ((CAN_3tq) << 16) | (((APB1_CLK/(CAN_TQS * CAN_BITRATE)) -1) & 0x3ff) ); // Set bit timingCAN1->FMR |= CAN_FMR_FINIT; // Set filter init, do default filter setup
CAN1->FMR &= ~CAN_FMR_CAN2SB; CAN1->FMR |= (CAN_FMR_CAN2SB & (0x1C << 8)); // all the filters to CAN1 can be used. CAN1->FM1R = 0x00000000; // Set all filters in Identifier mask mode CAN1->FS1R = 0x0fffffff; // Set all filters to 32 bit CAN1->FFA1R = 0x0aaaaaaa; // Even filters to FIFO0, odd filters to FIFO1 CAN1->FA1R = 0x00000000; // Disable all receive filters CAN1->FMR &= ~ CAN_FMR_FINIT; // Clear filter init NVIC_SetPriority(CAN1_RX0_IRQn,CAN_PRIO); NVIC_EnableIRQ(CAN1_RX0_IRQn); // Enable FIFO 0 interrupt NVIC_SetPriority(CAN1_RX1_IRQn,CAN_PRIO); NVIC_EnableIRQ(CAN1_RX1_IRQn); // Enable FIFO 1 interruptCAN1->MCR &= ~ CAN_MCR_INRQ; // End of initialization
GPIOB->BSRR = GPIO_BSRR_BR_6; // CAN_S low for(i = 0;i < CAN_NROF_RXMSG;i++){ can_buf_wptr[i] = 0; can_buf_rptr[i] = 0; }}// Setup and enable receive filter with index msg_index
void can_SetupFilter(UCHAR msg_index, UCHAR idsize, ULONG canid, ULONG mask){ULONG id_val, mask_val;volatile ULONG * can_filter_ptr;UCHAR filter_index;if (msg_index < CAN_NROF_FILTERS){
can_filter_ptr = &CAN1->sFilterRegister[0].FR1; // Pointer to first register in filter bank filter_index = msg_index * 2;if (idsize == CAN_STD_ID){
id_val = (canid << 21); mask_val = (mask << 21); } else { id_val = (canid << 3) | 0x04; // Id with IDE bit set mask_val = (mask << 3) | 0x04; }CAN1->FA1R &= ~ (1 << msg_index); // Deactivate filter
can_filter_ptr[filter_index] = id_val; // Set id
can_filter_ptr[filter_index+1] = mask_val; // Set maskCAN1->FA1R |= (1 << msg_index); // Activate filter
}}Solved! Go to Solution.
2017-06-28 6:38 PM
after investigated
a litlle further by studying the code ST uses in their standard peripheral library. It seems CAN2SB has to be in the range 1-27 not 28 as the RM says. When I set CAN2SB as 0x1B, it allows CAN1 using NO.0-26 filter banks.
2017-06-28 6:38 PM
after investigated
a litlle further by studying the code ST uses in their standard peripheral library. It seems CAN2SB has to be in the range 1-27 not 28 as the RM says. When I set CAN2SB as 0x1B, it allows CAN1 using NO.0-26 filter banks.