Question
flashing stm32F303 based custom board
Posted on May 03, 2018 at 23:36
Hello,
I am making a custom board based on STM32F3 discovery board. My custom board is an exact copy of the discovery board with additional sensor components.
I can easily program STM32F3 board as st-link is already built on to the board.
How do I do the same thing when I get my boards done?
I do have both
STM32F103C8T6
processor andSTM32F303VCT6
on the system.Is there a code for
STM32F103C8T6 which I can use to flash the board?
Can you please help me with this?
Best Regards,
Mallesh