Skip to main content
Bob Anderson
Associate
May 17, 2018
Question

TIMPRE HCLK multiplier in F413

  • May 17, 2018
  • 2 replies
  • 1043 views
Posted on May 17, 2018 at 11:08

In RM0430 rev 7 section 6.2 it is stated that when TIMPRE is set and APB prescaler is 1 or 2 then the timer clock is HCLK.

And when APB prescaler is > 2 then the timer clocks are HCLK * 4.

This is different to the F446 which in RM0390 section 6.2 which states that when APB prescaler is > 4 then timer clocks will be HCLK * 4.

So is the F413 indeed different as stated in the RM or is this a typo in the RM and the F413 is the same as the F446?

    This topic has been closed for replies.

    2 replies

    ST Technical Moderator
    May 17, 2018
    Posted on May 17, 2018 at 15:49

    Hello

    Anderson.Robert.002

    ,

    The F413 and

    F446

    products are different regarding this point and thereference manuals are correct.

    In fact, t

    he maximum

    HCLK frequency and the maximum APBs frequencies are not the same.

    With Regards,

    Imen

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
    Bob Anderson
    Associate
    May 17, 2018
    Posted on May 17, 2018 at 16:06

    Hi Imen.

    Thanks for the confirmation.

    Also another question will the next update of the Cube Eclipse plug-in implement the TIMPRE setting so that the clock configuration has the correct timer clocks when TIMPRE is set?

    Thanks,

    Bob