Skip to main content
Bob Anderson
Associate
May 6, 2018
Question

Error in RM0430 (rev 7)

  • May 6, 2018
  • 1 reply
  • 589 views
Posted on May 06, 2018 at 14:15

On page 177 the definition of bits 4:0 and 12:8 of RCC_DCKCFGR appear to be incorrect.

Should these be PLLI2SDIVQ and PLLSAIDIVQ respectively?

    This topic has been closed for replies.

    1 reply

    ST Technical Moderator
    May 11, 2018
    Posted on May 11, 2018 at 15:53

    H

    ello

    Anderson.Robert.002

    ,

    After check,there is a typo in the Bits 4:0PLLI2SDIVRDIVR

    , it should be PLLI2SDIVR.

    TheRCC_DCKCFGR register, bits 12:8 are used for the divider from PLL and should be called

    P

    LLDIVR.

    Best Regards,

    Imen

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks