Skip to main content
Zhiyong Wu
Associate II
July 13, 2017
Question

Use ST_Link Programmer from Nucleo 64 F411RE Board to program a Stand Alone STM32F411RE Chips

  • July 13, 2017
  • 10 replies
  • 4051 views
Posted on July 13, 2017 at 15:41

Hi, I have a ST_Link Programmer that was cut off from STM32F411RE Nucleo 64 Board (zero ohms resistors SB12, 13, 14, and 15 have been also removed). I have been use it to program other STM series Board with no problem.

Currently I am doing a project that is using STM32F411RE Nucleo 64 Board and I have a custom made PCB with STM32F411RE chips on it. I tried to use the same ST_Link Programmer to program the chips by connect the 8 pins from the programmer to the chips, but it does not work. The pins are connected the same as how I connect my programmer to the nucleo board.

When I connect the programmer to STM32F411RE Nucleo 64 Board:

Programmer

- - - - - - - - - - - - - - - - - - - - - - - - - - - - -

Board

Left Pin from JP1 (next to USB Power)- - - - - - -VDD (CN7-5)

SWCLK (CN4-2)- - - - - - - - - - - - - - - - - - - - - - - - -PA14 (CN7-15)

GND (CN4-3)- - - - - - - - - - - - - - - - - - - - - - - - - - -GND (CN7-8)

SWDIO (CN4-4)- - - - - - - - - - - - - - - - - - - - - - - - -PA13 (CN7-13)

NRST (CN4-5)- - - - - - - - - - - - - - - - - - - - - - - - - -NRST (CN7-14)

SWO (CN4-6)- - - - - - - - - - - - - - - - - - - - - - - - - - -PB3 (CN10-31)

TX (CN3-1)- - - - - - - - - - - - - - - - - - - - - - - - - - - - -PA3 - RX (CN10-37)

RX (CN3-2)- - - - - - - - - - - - - - - - - - - - - - - - - - - - -PA2 - TX (CN10-35)

With the connection above, I can program my Nucleo board with external ST-Link programmer that I cut off before. Everything works fine.

And then I connected the same programmer to my STM32F411RE Chips with the same pins as following:

Programmer

- - - - - - - - - - - - - - - - - - - - - - - - - - - -

STM32F411RE MCU

Left Pin from JP1 (next to USB Power)- - - - - - - - - - - -VDD (Pin 19)

SWCLK (CN4-2)- - - - - - - - - - - - - - - - - - - - - - - - - - - - - -PA14 (Pin 49)

GND (CN4-3)- - - - - - - - - - - - - - - - - - - - - - - - - - - - - - - -VSS (Pin 18)

SWDIO (CN4-4)- - - - - - - - - - - - - - - - - - - - - - - - - - - - - -PA13 (Pin 46)

NRST (CN4-5)- - - - - - - - - - - - - - - - - - - - - - - - - - - - - - -NRST (Pin 7)

SWO (CN4-6)- - - - - - - - - - - - - - - - - - - - - - - - - - - - - - - -PB3 (Pin 55)

TX (CN3-1)- - - - - - - - - - - - - - - - - - - - - - - - - - - - - - - - - -PA3 - RX (Pin 17)

RX (CN3-2)- - - - - - - - - - - - - - - - - - - - - - - - - - - - - - - - - -PA2 - TX (Pin 16)

This time, when I connect the program to my computer, same storage disk (NODE_F411RE (D:)) has jumped out, however, in stead of usual two files (

DETAILS.TXT and

MBED.HTM), there is one additional file called

FAIL.TXT, and when I opened it out, it shows:

The interface firmware FAILED to reset/halt the target MCU.

I am not sure how to fixed this, if anyone can help, that would be appreciated.

Thank you

Note: this post was migrated and contained many threaded conversations, some content may be missing.
    This topic has been closed for replies.

    10 replies

    Tesla DeLorean
    Guru
    July 13, 2017
    Posted on July 13, 2017 at 16:50

    More indicative of VDDA/VREF+ not being powered. Also want capacitors on VCAP pin(s).

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    Zhiyong Wu
    Associate II
    July 13, 2017
    Posted on July 13, 2017 at 17:18

    Hi, thanks for the reply. So do I connect Left Pin from JP1 (power) to VDDA/VREF+?  What is VCAP pin(s)? and what size of capacitors that I should use? Thank you.

    Tesla DeLorean
    Guru
    July 13, 2017
    Posted on July 13, 2017 at 17:46

    There's a manual for the part that's worth reviewing

    http://www.st.com/content/ccc/resource/technical/document/datasheet/b3/a5/46/3b/b4/e5/4c/85/DM00115249.pdf/files/DM00115249.pdf/jcr:content/translations/en.DM00115249.pdf

     

    Single VCAP pin (30) would need a 4u7F, it's the bulk capacitor for the 1.25V regulator powering the core. The VDDA/VREF+ powers the analogue circuitry (so POR and PLL/VCO as I recall), no power there device held in reset indefinitely.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..