Skip to main content
Edwin kaus
Associate III
November 20, 2017
Question

STM32F765 MCU Nand flash issue

  • November 20, 2017
  • 0 replies
  • 450 views
Posted on November 20, 2017 at 07:45

I am working on STM32F765BIT MCU with our custom board . In our board NAND flash is connected to Bank3 (0x80000000 - 0x8FFFFFFF). I configured using STM cube and just tried to read device ID but MCU is getting locked once I did that. Simply two MCU are locked while doing these experiment . 

I found that even internal Flash is also sharing same space, if so how can I access external NAND flash. Can anyone give some brief explanation how do I access external NAND flash. Is there any method to remap internal flash to other space. I just want to read/write external NAND flash for the first stage.

Also suggest is it possible to reuse those MCU once after locked, if so how to unlock those MCU.

Thank you., 

#nand-flash #stm32f7
This topic has been closed for replies.