Skip to main content
starlin lin
Associate
July 17, 2017
Question

RTC can't work because PLL already use

  • July 17, 2017
  • 2 replies
  • 649 views
Posted on July 17, 2017 at 07:46

Dear Sir:

I had reference the PWR_STANDBY_RTC sample code form STM32Cube_FW_L4_V1.8.0

This sample code are work well and wake up about 30 second,

but after move to my code get return fail at

if(HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK) form 

SystemClock_Config()

void SystemClock_Config(void)

{

......

RCC_OscInitStruct.PLL.PLLR = 2;

RCC_OscInitStruct.PLL.PLLP = 7;

RCC_OscInitStruct.PLL.PLLQ = 4;

if(HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)

{

// return here.

while(1);

}

after check, find is because PLL already used?

/* Check if the PLL is used as system clock or not */

if(__HAL_RCC_GET_SYSCLK_SOURCE() != RCC_CFGR_SWS_PLL)

{

.......

else

{

return HAL_ERROR;

}

I have reference this web say need turn off some content of 

SystemInit()

https://www.mianbaoban.cn/blog/post/45024

 

but still don't work, then how to use PLL and let SystemClock_Config?

Thx for your answer.

    This topic has been closed for replies.

    2 replies

    Vangelis Fortounas
    Associate II
    July 17, 2017
    Posted on July 17, 2017 at 11:37

    Hello

    Normaly  after reset (wkup reset after stby mode) the MSI is the default clock source .

    check the  standby flag  after reset to see if the mc was in StandBy Mode.

    __HAL_PWR_GET_FLAG(PWR_FLAG_SB);

    Clear this flag  after read it.

    starlin lin
    Associate
    July 17, 2017
    Posted on July 17, 2017 at 11:49

    thx for reply.

    at the sample code,

    int main(void)

    {

    HAL_Init();

    SystemClock_Config();

    BSP_LED_Init(LED2);

    RTC_Config();

    SystemPower_Config();

    if(__HAL_PWR_GET_FLAG(PWR_FLAG_SB) != RESET)

    {

    __HAL_PWR_CLEAR_FLAG(PWR_FLAG_SB);

    }

    .....

    I do the same thing, but return error from 

    SystemClock_Config();

    I have try move clear sb flag to up then SystemClock_Config(), but get same result.

    BTW, my project is base on zephyr RTOS.