Skip to main content
guo qiang
Senior
August 28, 2017
Question

The portMacro.h of FreeRTOS

Posted on August 28, 2017 at 06:15

0690X000006081uQAA.png

The MPC series is a 32-bit chip.Why is FreeRTOS portSTACK_TYPE defined as a long type? I think it should be uint32 type.

Because STM32 is 32-bit chip, STM32 inside the portSTACK_TYPE defined as uint32 type
    This topic has been closed for replies.

    2 replies

    guo qiang
    guo qiangAuthor
    Senior
    August 28, 2017
    Posted on August 28, 2017 at 06:17

    long is 4Bytes in the  MPC? 

    or 8Bytes?

    Erwan YVIN
    ST Technical Moderator
    August 28, 2017
    Posted on August 28, 2017 at 10:02

    Hello Guo ,

    Long should be 4 bytes in MPC 32 Bits

      

          Best regards

             Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.