Skip to main content
eddie McS
Associate II
August 8, 2017
Solved

How to get S2-LP into CW mode?

  • August 8, 2017
  • 2 replies
  • 1198 views
Posted on August 08, 2017 at 14:40

Hi,

I have the ST S2-LP transceiver both transmitting and receiving just fine however i'm struggling to put the chip into a continuous wave mode.. 

from reading the data sheet i have configure the following : 

  • To set the continuous wave the TXSOURCE field (of the PCKTCTRL1 register) must be set to 0x03
  • To set the continuous wave the MOD_TYPE field (of the MOD2 register) must be set to 0x70

Is there any additional registers i should be aware of in order to configure continuous wave mode?

Thanks

Ed

    This topic has been closed for replies.
    Best answer by eddie McS
    Posted on August 10, 2017 at 16:40

    I forgot to start transmitting...

    S2LPCmdStrobeTx();

    All works now

    2 replies

    eddie McS
    eddie McSAuthorBest answer
    Associate II
    August 10, 2017
    Posted on August 10, 2017 at 16:40

    I forgot to start transmitting...

    S2LPCmdStrobeTx();

    All works now

    DInga.1
    Visitor II
    October 13, 2020

    Hi Eddie,

    Were there any steps before sending these commands.

    I used the S2LP libraries like this:

    S2LP_RADIO_SetModulation( MOD_NO_MOD);

    S2LP_PCKT_HNDL_SetTxMode(PN9_TX_MODE);

    S2LP_CMD_StrobeTx();

    But no TX happening.

    It's flagging a Hard Fault Interrupt.

    I tried to initialize the radio by copying some codes from the example under X-CUBE-SUBG2 package.

    But still no luck.

    Any help will be appreciated.

    Regards,

    Dominique