Skip to main content
Mohamed Osama
Associate
July 29, 2017
Question

stm8l151c8 Interrupt is not working

  • July 29, 2017
  • 1 reply
  • 1270 views
Posted on July 29, 2017 at 15:58

Hi,

I'm using stm8l151c8 controller, I'm trying to get an interrupt from PB0 but it's not working, here is my code:

&sharpinclude 'stm8l15x_conf.h'

&sharpinclude 'main.h'

uint8_t __IO BlinkSpeed = 0;

static __IO uint32_t TimingDelay;

void Delay(__IO uint32_t nCount)

{

while(nCount--)

{

}

}

void TimingDelay_Decrement(void)

{

if (TimingDelay != 0x00)

{

TimingDelay--;

}

}

uint8_t data_audio,data_transmit;

uint8_t get_bit(uint8_t bits, uint8_t pos)

{

return (bits >> pos) & 0x01;

}

&sharppragma vector=0x008028

@svlreg @interrupt void EXTI0_IRQHandler()

{

uint8_t i=0;

if (EXTI_GetITStatus(EXTI_IT_Pin0) != RESET) {

Delay(3);

for(i=0;i<8;i++)

{

data_audio=data_audio<<0x01;

data_audio=data_audio|GPIO_ReadInputDataBit(GPIOB,GPIO_Pin_0);

Delay(5);

}

for(i=0;i<8;i++)

{

data_transmit=get_bit(data_audio,7-i);

if(data_transmit==0x00)

GPIO_WriteBit(GPIOD,GPIO_Pin_2,0x00);

else

GPIO_WriteBit(GPIOD,GPIO_Pin_2,0x01);

Delay(10);

}

// Clear interrupt flag

EXTI_ClearITPendingBit(EXTI_IT_Pin0);

}

}

void GPIO_cnfg()

{

GPIO_Init(GPIOD,GPIO_Pin_2,GPIO_Mode_Out_PP_Low_Fast);

GPIO_Init(GPIOB,GPIO_Pin_0,GPIO_Mode_In_FL_IT);

EXTI_SelectPort(EXTI_Port_B);

EXTI_SetHalfPortSelection(EXTI_HalfPort_B_LSB, ENABLE);

EXTI_SetPortSensitivity( EXTI_Port_B, EXTI_Trigger_Rising);

EXTI_SetPinSensitivity(EXTI_IT_Pin0, EXTI_Trigger_Rising);

enableInterrupts();

}

static void CLK_Config(void)

{

/* Select HSE as system clock source */

CLK_SYSCLKSourceSwitchCmd(ENABLE);

CLK_HSICmd(ENABLE);

CLK_SYSCLKSourceConfig(CLK_SYSCLKSource_HSI);

/* system clock prescaler: 1*/

CLK_SYSCLKDivConfig(CLK_SYSCLKDiv_1);

while (CLK_GetSYSCLKSource() != CLK_SYSCLKSource_HSI)

{}

}

int main (void) {

CLK_Config();

GPIO_cnfg();

while(1) { 

               }

}

&sharpifdef USE_FULL_ASSERT

void assert_failed(uint8_t* file, uint32_t line)

{

while (1)

{

}

}

&sharpendif

and here is stm8_interrupt_vector.c

&sharpinclude 'main.h'

typedef void @far (*interrupt_handler_t)(void);

struct interrupt_vector {

unsigned char interrupt_instruction;

interrupt_handler_t interrupt_handler;

};

@far @interrupt void NonHandledInterrupt (void)

{

return;

}

extern void _stext(); /* startup routine */

extern void EXTI0_IRQHandler();

struct interrupt_vector const _vectab[] = {

{0x82, (interrupt_handler_t)_stext}, /* reset */

{0x82, NonHandledInterrupt}, /* trap */

{0x82, (interrupt_handler_t)EXTI0_IRQHandler}, /* irq0 */

{0x82, NonHandledInterrupt}, /* irq1 */

{0x82, NonHandledInterrupt}, /* irq2 */

{0x82, NonHandledInterrupt}, /* irq3 */

{0x82, NonHandledInterrupt}, /* irq4 */

{0x82, NonHandledInterrupt}, /* irq5 */

{0x82, NonHandledInterrupt}, /* irq6 */

{0x82, NonHandledInterrupt}, /* irq7 */

{0x82, NonHandledInterrupt}, /* irq8 */

{0x82, NonHandledInterrupt}, /* irq9 */

{0x82, NonHandledInterrupt}, /* irq10 */

{0x82, NonHandledInterrupt}, /* irq11 */

{0x82, NonHandledInterrupt}, /* irq12 */

{0x82, NonHandledInterrupt}, /* irq13 */

{0x82, NonHandledInterrupt}, /* irq14 */

{0x82, NonHandledInterrupt}, /* irq15 */

{0x82, NonHandledInterrupt}, /* irq16 */

{0x82, NonHandledInterrupt}, /* irq17 */

{0x82, NonHandledInterrupt}, /* irq18 */

{0x82, NonHandledInterrupt}, /* irq19 */

{0x82, NonHandledInterrupt}, /* irq20 */

{0x82, NonHandledInterrupt}, /* irq21 */

{0x82, NonHandledInterrupt}, /* irq22 */

{0x82, NonHandledInterrupt}, /* irq23 */

{0x82, NonHandledInterrupt}, /* irq24 */

{0x82, NonHandledInterrupt}, /* irq25 */

{0x82, NonHandledInterrupt}, /* irq26 */

{0x82, NonHandledInterrupt}, /* irq27 */

{0x82, NonHandledInterrupt}, /* irq28 */

{0x82, NonHandledInterrupt}, /* irq29 */

};

main.h file includes only the prototype of the interrupt function:

@svlreg @interrupt void EXTI0_IRQHandler();

every time it calls nonhandled interrupt function, but the address I'm putting in pragma vector line is correct, it's weird, I guess there is something missing.

Thank you for your help.

#stm8s-interrupt #interrupt #interrupt-issue
This topic has been closed for replies.

1 reply

Mohamed Osama
Associate
July 30, 2017
Posted on July 30, 2017 at 16:31

the correct one is to write the function for handling interrupt at the correct location in the stm8_vector_table, that's the solution.