Skip to main content
ryan nguyen
Associate
November 13, 2017
Question

STM32F303 Nucleo CAN HAL_TIMEOUT Error

  • November 13, 2017
  • 1 reply
  • 649 views
Posted on November 13, 2017 at 09:38

Hello,

I'm trying to set up CAN on my STM32F303 nucleoy board to send a CAN message but I keep getting HAL_TIMEOUT error from the HAL_CAN_Transmit() function. Here's my code:

/**

******************************************************************************

*/

/* Includes ------------------------------------------------------------------*/

#include 'main.h'

#include 'stm32f3xx_hal.h'

CAN_HandleTypeDef hcan;

void SystemClock_Config(void);

static void MX_GPIO_Init(void);

static void MX_CAN_Init(void);

int main(void)

{

/* MCU Configuration----------------------------------------------------------*/

/* Reset of all peripherals, Initializes the Flash interface and the Systick. */

HAL_Init();

/* Configure the system clock */

SystemClock_Config();

/* Initialize all configured peripherals */

MX_GPIO_Init();

MX_CAN_Init();

/* Infinite loop */

HAL_StatusTypeDef status;

while (1)

{

hcan.pTxMsg->Data[0] = 1;

hcan.pTxMsg->Data[1] = 2;

status = HAL_CAN_Transmit(&hcan, 10);

HAL_GPIO_WritePin(GPIOA, GPIO_PIN_1, GPIO_PIN_RESET);

}

}

/** System Clock Configuration

*/

void SystemClock_Config(void)

{

RCC_OscInitTypeDef RCC_OscInitStruct;

RCC_ClkInitTypeDef RCC_ClkInitStruct;

/**Initializes the CPU, AHB and APB busses clocks

*/

RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;

RCC_OscInitStruct.HSIState = RCC_HSI_ON;

RCC_OscInitStruct.HSICalibrationValue = 16;

RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;

RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI;

RCC_OscInitStruct.PLL.PLLMUL = RCC_PLL_MUL8;

if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)

{

_Error_Handler(__FILE__, __LINE__);

}

/**Initializes the CPU, AHB and APB busses clocks

*/

RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK

|RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;

RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;

RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV2;

RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;

RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;

if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_0) != HAL_OK)

{

_Error_Handler(__FILE__, __LINE__);

}

/**Configure the Systick interrupt time

*/

HAL_SYSTICK_Config(HAL_RCC_GetHCLKFreq()/1000);

/**Configure the Systick

*/

HAL_SYSTICK_CLKSourceConfig(SYSTICK_CLKSOURCE_HCLK);

/* SysTick_IRQn interrupt configuration */

HAL_NVIC_SetPriority(SysTick_IRQn, 0, 0);

}

/* CAN init function */

static void MX_CAN_Init(void)

{

CAN_FilterConfTypeDef sFilterConfig;

static CanTxMsgTypeDef TxMessage;

static CanRxMsgTypeDef RxMessage;

hcan.pTxMsg = &TxMessage;

hcan.pRxMsg = &RxMessage;

hcan.Instance = CAN;

hcan.Init.Prescaler = 8;

hcan.Init.Mode = CAN_MODE_NORMAL;

hcan.Init.SJW = CAN_SJW_1TQ;

hcan.Init.BS1 = CAN_BS1_1TQ;

hcan.Init.BS2 = CAN_BS2_2TQ;

hcan.Init.TTCM = DISABLE;

hcan.Init.ABOM = DISABLE;

hcan.Init.AWUM = DISABLE;

hcan.Init.NART = DISABLE;

hcan.Init.RFLM = DISABLE;

hcan.Init.TXFP = DISABLE;

if (HAL_CAN_Init(&hcan) != HAL_OK)

{

_Error_Handler(__FILE__, __LINE__);

}

/*##-2- Configure the CAN Filter ###########################################*/

sFilterConfig.FilterNumber = 0;

sFilterConfig.FilterMode = CAN_FILTERMODE_IDMASK;

sFilterConfig.FilterScale = CAN_FILTERSCALE_32BIT;

sFilterConfig.FilterIdHigh = 0x0000;

sFilterConfig.FilterIdLow = 0x0000;

sFilterConfig.FilterMaskIdHigh = 0x0000;

sFilterConfig.FilterMaskIdLow = 0x0000;

sFilterConfig.FilterFIFOAssignment = 0;

sFilterConfig.FilterActivation = ENABLE;

sFilterConfig.BankNumber = 14;

if (HAL_CAN_ConfigFilter(&hcan, &sFilterConfig) != HAL_OK)

{

/* Filter configuration Error */

Error_Handler();

}

/*##-3- Configure Transmission process #####################################*/

hcan.pTxMsg->StdId = 0x3;

hcan.pTxMsg->ExtId = 0x01;

hcan.pTxMsg->RTR = CAN_RTR_DATA;

hcan.pTxMsg->IDE = CAN_ID_STD;

hcan.pTxMsg->DLC = 2;

}

/** Configure pins as

* Analog

* Input

* Output

* EVENT_OUT

* EXTI

*/

static void MX_GPIO_Init(void)

{

GPIO_InitTypeDef GPIO_InitStruct;

/* GPIO Ports Clock Enable */

__HAL_RCC_GPIOA_CLK_ENABLE();

/*Configure GPIO pin Output Level */

HAL_GPIO_WritePin(GPIOA, GPIO_PIN_1|GPIO_PIN_2, GPIO_PIN_RESET);

/*Configure GPIO pins : PA1 PA2 */

GPIO_InitStruct.Pin = GPIO_PIN_1|GPIO_PIN_2;

GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;

GPIO_InitStruct.Pull = GPIO_NOPULL;

GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;

HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);

}

/* USER CODE BEGIN 4 */

/* USER CODE END 4 */

/**

* @brief This function is executed in case of error occurrence.

* @param None

* @retval None

*/

void _Error_Handler(char * file, int line)

{

/* USER CODE BEGIN Error_Handler_Debug */

/* User can add his own implementation to report the HAL error return state */

while(1)

{

}

/* USER CODE END Error_Handler_Debug */

}

#ifdef USE_FULL_ASSERT

/**

* @brief Reports the name of the source file and the source line number

* where the assert_param error has occurred.

* @param file: pointer to the source file name

* @param line: assert_param error line source number

* @retval None

*/

void assert_failed(uint8_t* file, uint32_t line)

{

/* USER CODE BEGIN 6 */

/* User can add his own implementation to report the file name and line number,

ex: printf('Wrong parameters value: file %s on line %d\r\n', file, line) */

/* USER CODE END 6 */

}

#endif

Any help is appreciated!

Thank you

    This topic has been closed for replies.

    1 reply

    ST Technical Moderator
    November 15, 2017
    Posted on November 15, 2017 at 15:18

    Hello,

    W

    hich Cube firmware package are you using ?

    Ensure to use the last version of STM32CubeF3 as contains fix about HAL_CAN_Transmit

     function reach timeout.

    Best Regards

    Imen

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks