Skip to main content
R0b0t1 R0b0t1
Associate II
May 12, 2018
Question

Help setting up X-CUBE-MEMSMIC1 demo for NUCLEO-L476RG and X-NUCLEO-CCA02M1

  • May 12, 2018
  • 0 replies
  • 539 views
Posted on May 12, 2018 at 07:33

Hello,

Unfortunately, I am having problems with the demo included in the X-CUBE-MEMSMIC1 package for the NUCLEO-L476RG. After loading the precompiled file to the board and attempting to plug it in to a computer via the X-NUCLEO-CCA02M1's connector, the device does not register with my computer (Linux or Windows). Can any troubleshooting advice be given?

I have not modified the jumpers on the board. Is my reading of the manual correct, and that I need to set the jumpers to DFSDM operation to use the pregenerated files (which as far as I can tell select DFSDM operation on the L476RG board)? Would this cause a failure to enumerate?

Thanks in advance!

#nucleo-l476rg #audio #microphone
This topic has been closed for replies.