Question
VL53L0X inialisation failing in PerfomRefSpadManagment
Posted on October 05, 2017 at 07:00
Debugging shows it fails due to error in the VL53L0X_REG_RESULT_INTERRUPT_STATUS register read in VL53L0X_GetInterruptMaskStatus.
Can anyone tell me what values 0x50, 0x54 and 0x4C describe and how to resolve it?
My stack is:
VL53L0X_GetInterruptMaskStatus() at vl53l0x_api.c:2,911 0x800510c
VL53L0X_GetMeasurementDataReady() at vl53l0x_api.c:2,335 0x8005138 VL53L0X_measurement_poll_for_completion() at vl53l0x_api_core.c:72 0x800591e VL53L0X_perform_single_ref_calibration() at vl53l0x_api_calibration.c:1,076 0x8005438 VL53L0X_perform_vhv_calibration() at vl53l0x_api_calibration.c:1,144 0x800555a VL53L0X_perform_ref_calibration() at vl53l0x_api_calibration.c:1,227 0x800562c VL53L0X_perform_ref_spad_management() at vl53l0x_api_calibration.c:763 0x80056e8 VL53L0X_PerformRefSpadManagement() at vl53l0x_api.c:3,034 0x800517a TOF_InitSensor() at main.c:287 0x800c44aThe Initialisation code to that point looks like:
static const uint8_t i2cInitialAddress = 0x52; // LSB is reserved
uint8_t i2cFinalAddress = 0x60;memset(tofSens, 0, sizeof(VL53L0X_Dev_t));tofSens->I2cDevAddr = i2cInitialAddress;tofSens->comms_type = 1;tofSens->comms_speed_khz = 100;VL53L0X_SetDeviceAddress(tofSens, i2cFinalAddress);tofSens->I2cDevAddr = i2cFinalAddress;VL53L0X_DataInit(tofSens); //Success!VL53L0X_StaticInit(tofSens); //Success!uint32_t refSpadCount;uint8_t isApertureSpads;VL53L0X_PerformRefSpadManagement(tofSens, &refSpadCount, &isApertureSpads); // FAILSI'm communicating fine with the device with I2C.
#vl53l0x