Skip to main content
MDW
Associate II
December 5, 2017
Question

stm32l0x1 incorrect UID LL_driver

  • December 5, 2017
  • 1 reply
  • 605 views
Posted on December 05, 2017 at 15:47

In the stm32l0xx_ll_utils.h, the UID is using the wrong offset:

__STATIC_INLINE uint32_t LL_GetUID_Word2(void)

{

  return (uint32_t)(READ_REG(*((uint32_t *)(UID_BASE_ADDRESS + 8U))));

}

Checked in both STM32Cube_FW_L0_V1.9.0 and STM32Cube_FW_L0_V1.10.0

In the reference manual (RM0377.pdf) page 818 the offset is defined as 0x14 which seems to work.

Could someone verify this or send me to the correct channel to submit this driver-bug?

#stm32l0x1 #uid #driver-bug
This topic has been closed for replies.

1 reply

ST Technical Moderator
December 26, 2017
Posted on December 26, 2017 at 14:46

Hello

De_Witte.Michiel

,

Thank you for your bug reporting.

I confirm this issue of the STM32L0 HAL which defined incorrect unique device ID.

This issue is already raised internally to the appropriate team.

Kind Regards,

Imen.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks