Skip to main content
Kim ElQ
Associate II
September 5, 2017
Question

Icube_LRWAN ( End_node)

  • September 5, 2017
  • 0 replies
  • 421 views
Posted on September 05, 2017 at 12:15

Hello , 

i'm using murata's module CMWX1ZZabz including stm32l0,  with the provided lorawan_cube code , here is the lowpower_handler fontion, anyone has an idea how to control the MCU wakeup.

in addition to that, the consumption is high in sleep_mode : 1.5mA instead of ~5uA .

Thank you

void LowPower_Handler( void )

{

DBG_GPIO_RST(GPIOB, GPIO_PIN_15);

DBG_GPIO_RST(GPIOB, GPIO_PIN_14);

if ( LowPower_State == 0 )

   {

         HW_EnterStopMode( );

         /* mcu dependent. to be implemented by user*/

         HW_ExitStopMode();

         DBG_GPIO_SET(GPIOB, GPIO_PIN_15);

         HW_RTC_setMcuWakeUpTime( );

   }

else

   {   

         DBG_PRINTF_CRITICAL('z\n\r');

         HW_EnterSleepMode( );

         DBG_GPIO_SET(GPIOB, GPIO_PIN_14);

   }

}
    This topic has been closed for replies.