Standby mode current consumption is not reduced to expected value
- August 29, 2017
- 4 replies
- 5828 views
Hello everyone, I am trying to measure the current consumption in STM32L011F4 microcontroller. I tried the STANDBY mode sample code provide by STM in 'stm32cubel0'. Standby mode current consumption is about 320�A when I measured it using a multimeter. The datasheet says that the maximum current consumption is 0.6�A for temperature between -40�C to 25�C with Independent watchdog and LSI OFF. The code is shown below. Does anyone have an idea why the current consumption is more that expected?
int main(void)
{ /* STM32L0xx HAL library initialization */ HAL_Init();/* Configure the system clock to 2 MHz */
SystemClock_Config();/* System Power Configuration */
SystemPower_Config() ; /* Check if the system was resumed from Standby mode */ if (__HAL_PWR_GET_FLAG(PWR_FLAG_SB) != RESET) { /* Clear Standby flag */ __HAL_PWR_CLEAR_FLAG(PWR_FLAG_SB); }/* Insert 5 seconds delay */
HAL_Delay(5000);/* The Following Wakeup sequence is highly recommended prior to each Standby mode entry
mainly when using more than one wakeup source this is to not miss any wakeup event. - Disable all used wakeup sources, - Clear all related wakeup flags, - Re-enable all used wakeup sources, - Enter the Standby mode. *//* Disable all used wakeup sources: PWR_WAKEUP_PIN3 */
HAL_PWR_DisableWakeUpPin(PWR_WAKEUP_PIN3);/* Clear all related wakeup flags*/
__HAL_PWR_CLEAR_FLAG(PWR_FLAG_WU); /* Enable WakeUp Pin PWR_WAKEUP_PIN3 connected to PA.02 (Arduino A7) */ HAL_PWR_EnableWakeUpPin(PWR_WAKEUP_PIN3);/* Enter the Standby mode */
HAL_PWR_EnterSTANDBYMode();/* This code will never be reached! */
while (1) { }}/**
* @brief System Clock Configuration * The system Clock is configured as follow : * System Clock source = MSI * SYSCLK(Hz) = 2000000 * HCLK(Hz) = 2000000 * AHB Prescaler = 1 * APB1 Prescaler = 1 * APB2 Prescaler = 1 * Flash Latency(WS) = 0 * Main regulator output voltage = Scale3 mode * @retval None */void SystemClock_Config(void){ RCC_ClkInitTypeDef RCC_ClkInitStruct = {0}; RCC_OscInitTypeDef RCC_OscInitStruct = {0}; /* Enable MSI Oscillator */ RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_MSI; RCC_OscInitStruct.MSIState = RCC_MSI_ON; RCC_OscInitStruct.MSIClockRange = RCC_MSIRANGE_5; RCC_OscInitStruct.MSICalibrationValue=0x00; RCC_OscInitStruct.PLL.PLLState = RCC_PLL_NONE; if (HAL_RCC_OscConfig(&RCC_OscInitStruct)!= HAL_OK) { /* Initialization Error */ while(1); } /* Select MSI as system clock source and configure the HCLK, PCLK1 and PCLK2 clocks dividers */ RCC_ClkInitStruct.ClockType = (RCC_CLOCKTYPE_SYSCLK | RCC_CLOCKTYPE_HCLK | RCC_CLOCKTYPE_PCLK1 | RCC_CLOCKTYPE_PCLK2); RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_MSI; RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1; RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1; RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1; if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_0)!= HAL_OK) { /* Initialization Error */ while(1); } /* Enable Power Control clock */ __HAL_RCC_PWR_CLK_ENABLE(); /* The voltage scaling allows optimizing the power consumption when the device is clocked below the maximum system frequency, to update the voltage scaling value regarding system frequency refer to product datasheet. */ __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE3); /* Disable Power Control clock */ __HAL_RCC_PWR_CLK_DISABLE(); }/**
* @brief System Power Configuration * The system Power is configured as follow : * + VREFINT OFF, with fast wakeup enabled * + No IWDG * + Wakeup using PWR_WAKEUP_PIN3 * @param None * @retval None */static void SystemPower_Config(void){ /* Enable Power Control clock */ __HAL_RCC_PWR_CLK_ENABLE();/* Enable Ultra low power mode */
HAL_PWREx_EnableUltraLowPower(); /* Enable the fast wake up from Ultra low power mode */ HAL_PWREx_EnableFastWakeUp();}#current-consumption #stm32 #stm32l0 #standby-mode