2017-09-07 2:42 AM
Hi
I want to know, what is the difference between stmcube and SPL? Has SPL replaced by stmcube? or stmcube is something above the SPL? cause I think there is another thing called HAL library!
Also, when I want to use CMSIS-Core I should use which one of them, If I like to have low level access to registers?
I have stm32f40vg discovery board that I bought 4years ago, and like to use CMSIS-Core for programming, but I understood SPL is outdated and not supported for now! So what is the alternative for SPL? Or can I use SPL yet?
Solved! Go to Solution.
2017-09-07 5:54 AM
Hi,
Have a look to
.If you still have confusion even after that, please let me know what exactly needs clarification.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2017-09-07 5:54 AM
Hi,
Have a look to
.If you still have confusion even after that, please let me know what exactly needs clarification.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2017-09-07 8:15 AM
HAL replaces SPL, CubeMX is a code generator targetting HAL compatible output.
SPL continues to be supported by those that matter, is doesn't need constant iteration because it isn't packed full of bugs/pitfalls. The SPL for the F4 will continue to work reliably for years to come. If you expect to be building something with a 5-10 year product life, which you will be expected to support/service, where field updates are difficult/impractical, use the SPL, it is far less likely to bite you.
If you enjoy the Microsoft/Adobe software update/delivery model of constant churn and regression, chose HAL
2017-09-07 8:22 AM
Thank you Amel,
But, what about CMSIS? CMSIS is which part of this story?
2017-09-07 10:34 AM
CMSIS header files are available in both packages (Cube and SPL).
Both development approaches allow you to have low level access to register (this wasn't easy to do with HAL -High Abstraction Layer- drivers embedded in the Cube package, but is facilitated since the LL -Low Layer- drivers were added).
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.