Skip to main content
Robert Wollner
Associate
September 6, 2017
Question

Nucleo STM32F207ZG Ethernet problem DHCP on LWIP using CubeMX

  • September 6, 2017
  • 2 replies
  • 934 views
Posted on September 06, 2017 at 17:24

Why does the default code hang on DHCP response?

Took a while to sift through the STM32cubeMX autogenerated code. Writing a question here to make it searchable and findable by others.

When turning on all the relavant options and sorting out a normal/default code base to begin a project, the project just hangs.

#stm32f207 #nucleo #lwip #dhcp
This topic has been closed for replies.

2 replies

Robert Wollner
Associate
September 6, 2017
Posted on September 06, 2017 at 17:28

Replying to my own question to answer for others:

in the file 'FreeRTOS/Source/portable/GCC/ARM_CM3/port.c' there's a function call to configASSERT within the vPortValidateInterruptPriority function..

It's supposed to check whether the uCurrentPriority is <= ucMaxSysCallPriority, however the comparison operatior is backwards.

Change this from >= to <= and the program will work as normal.

Nicholas Hemstreet
Associate
June 15, 2018
Posted on June 15, 2018 at 22:09

Adding for visibility. I don't know the answer to your question, however I do know you need to make sure that RMII_TX_EN and RMII_TXD0 are configured to PG11 and PG13 respectively. CubeMX (v4.26 Cube v1.0 on Ubuntu Linux) configures them to the wrong pins. Already makes me wish we'd gone with Processor Expert.