Skip to main content
Rad Rad
Associate II
March 7, 2018
Question

ST7735 display driver usage

  • March 7, 2018
  • 2 replies
  • 2584 views
Posted on March 07, 2018 at 08:10

Hi .

I have a LCD display with st7735 and wanted to use library included within STM32Cube_FW_F3_V1.8.0 package.

Unfortunately the lib seems to be written only for specific boards and while compiling the code I get errors:

st7735.c:241: undefined reference to `LCD_IO_WriteReg'

/st7735.c:323: undefined reference to `LCD_IO_WriteMultipleData'

Is there a way to run it or a lib that would suit to STM32Cube HAL?

    This topic has been closed for replies.

    2 replies

    Amel NASRI
    ST Technical Moderator
    March 7, 2018
    Posted on March 07, 2018 at 10:21

    Hi

    Rad.Rad

    ‌,

    Do you have already suitable driver for ST7735? If not, you find them under STM32Cube_FW_F3_V1.9.0\Drivers\BSP\Components\st77

    This component is used in the demonstration provided for

    STM32F303ZE-Nucleo, which is available under

    STM32Cube_FW_F3_V1.9.0\Projects\STM32F303ZE-Nucleo\Demonstrations\Adafruit_LCD_1_8_SD_Joystick\Src\main.c.

    You need to refer to this example and adapt for your need.

    May I know with which hw will you be using this LCD display?

    -Amel

    To give better visibility on the answered topics, please click on "Best Answer" on the reply which solved your issue or answered your question.
    Rad Rad
    Rad RadAuthor
    Associate II
    March 21, 2018
    Posted on March 21, 2018 at 15:20

    Hi Amel,

    Thanks for your reply.

    I am using lib from: ...STM32Cube_FW_F3_V1.8.0\Projects\STM32F303RE-Nucleo\Demonstrations\Adafruit_LCD_1_8_SD_Joystick.

    However as I wrote is seems to be written for a nucleo board specyfic and throws the following errors:

    st7735.c:241: undefined reference to `LCD_IO_WriteReg'

    /st7735.c:323: undefined reference to `LCD_IO_WriteMultipleData'

    which I am not quite able to get over.

    I am using Arduino TFT: 

    https://www.arduino.cc/en/Guide/TFT