Skip to main content
Taras Koval
Visitor II
September 12, 2017
Question

stm32f030k6 problem with sysclk

  • September 12, 2017
  • 0 replies
  • 443 views
Posted on September 12, 2017 at 19:21

part of code from CoIDE

//----------Clock configure-------------//

RCC->CFGR |= RCC_CFGR_PLLMULL4;          // PLL multiplication factor = 4

RCC->CR |= RCC_CR_PLLON; // PLL start

RCC->CFGR |= RCC_CFGR_SW_PLL;             // PLL as SYCLK

RCC->CFGR |= RCC_CFGR_MCO_PLL;

//or sysclk       //RCC->CFGR |= RCC_CFGR_MCO_SYSCLK;

RCC->CFGR |= RCC_CFGR_MCO_PRE_16;    //mco div 16

HSI=8Mhz

8MHz/2(prediv)*4(pllmull)=16MHz

... but frequency meter show 6Mhz on MCO!!! even when MCO_PRE_16.

6x16=96!!! Is it real sysclk=96MHz?

When MCO_PRE is equal 64 MCO freq is 1.5MHz-->and again sysclk=96MHz

...when i put HSI or HSE to MCO, all work good and MCO out shows real freq

Then i used timer...

//----------TIM14 configure-------------//

TIM14->PSC = 16000;

TIM14->ARR = 1000;

TIM14->CR1 |= TIM_CR1_CEN;

TIM14->DIER |= TIM_DIER_UIE;

NVIC_EnableIRQ(TIM14_IRQn);

... interrupt was calld 6 times per seconds)))

16000x1000=16M clock cycles

16Mx6Hz(interrupt)=96MHz!!!

Is it real, or where my mistake?

    This topic has been closed for replies.