CAN2 interrupt not working
Hey guys,
I've got some issues with the CAN2 interrupt on the STM32F107 controller, I don't getan interrupt.
I'm using CubeMX and a STM32F10C Eval board.
First I tried CAN1 an this works fine so far. Everytime there is a message on the CAN Bus, I get an interrupt and can read out the data.
Then I configuried CAN2 in CubeMX with the same parameter as CAN1, and I have left CAN1 active.
I know that I need CAN1 active to use CAN2, because CAN2 hasn't direct access to the SRAM.
I also enabled RX0 and RX1 interrupt.
Then I add this lines to my main() function:
if(HAL_CAN_Receive_IT(&hcan2, CAN_FIFO0) != HAL_OK)
{
Error_Handler();
}�?�?�?�?
Andafter all I configuried the Filter for CAN2:
CAN_FilterConfTypeDef sFilterConfig;
hcan2.Instance = CAN2;
hcan2.pTxMsg = &TxMessage;
hcan2.pRxMsg = &RxMessage;
sFilterConfig.FilterNumber = 0;
sFilterConfig.FilterMode = CAN_FILTERMODE_IDMASK;
sFilterConfig.FilterScale = CAN_FILTERSCALE_32BIT;
sFilterConfig.FilterIdHigh = 0x0000;
sFilterConfig.FilterIdLow = 0x0000;
sFilterConfig.FilterMaskIdHigh = 0x0000;
sFilterConfig.FilterMaskIdLow = 0x0000;
sFilterConfig.FilterFIFOAssignment = 0;
sFilterConfig.FilterActivation = ENABLE;
sFilterConfig.BankNumber = 0;
if(HAL_CAN_ConfigFilter(&hcan2, &sFilterConfig) != HAL_OK)
{
Error_Handler();
}�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?
I just want to use CAN2, because of that I set the BankNumber to 0, which (I think) means, that every bank is available for CAN2.
And here is my interrupt routine:
void HAL_CAN_RxCpltCallback(CAN_HandleTypeDef* hcan)
{
HAL_GPIO_TogglePin(LED_BLUE_GPIO_Port, LED_BLUE_Pin);
if(HAL_CAN_Receive_IT(hcan, CAN_FIFO0) != HAL_OK)
{
Error_Handler();
}
}�?�?�?�?�?�?�?�?�?
Sending data on CAN2 is no problem, this works fine.
I also see on the oscilloscope that the transceiver is transmitting the data to the controller.
When I change hcan2 to hcan1, then I can use this code with CAN1, which workes fine.
In both cases I have configuried CAN1 and CAN2 with CubeMX.
Where could be my mistake?
Thank you