Skip to main content
Kang Sung Gu
Associate II
September 15, 2017
Question

STM32F429 NVIC Register Question

  • September 15, 2017
  • 4 replies
  • 1068 views
Posted on September 15, 2017 at 15:03

I want to know the NVIC Register

There is a description of GPIO and INTERRUPT in the Reference DataSheet, but there is no description of NVIC Register

Where can I find the details of the Register below?

typedef struct

{

  __IOM uint32_t ISER[8U];               /*!< Offset: 0x000 (R/W)  Interrupt Set Enable Register */

        uint32_t RESERVED0[24U];

  __IOM uint32_t ICER[8U];               /*!< Offset: 0x080 (R/W)  Interrupt Clear Enable Register */

        uint32_t RSERVED1[24U];

  __IOM uint32_t ISPR[8U];               /*!< Offset: 0x100 (R/W)  Interrupt Set Pending Register */

        uint32_t RESERVED2[24U];

  __IOM uint32_t ICPR[8U];               /*!< Offset: 0x180 (R/W)  Interrupt Clear Pending Register */

        uint32_t RESERVED3[24U];

  __IOM uint32_t IABR[8U];               /*!< Offset: 0x200 (R/W)  Interrupt Active bit Register */

        uint32_t RESERVED4[56U];

  __IOM uint8_t  IP[240U];               /*!< Offset: 0x300 (R/W)  Interrupt Priority Register (8Bit wide) */

        uint32_t RESERVED5[644U];

  __OM  uint32_t STIR;                   /*!< Offset: 0xE00 ( /W)  Software Trigger Interrupt Register */

}  NVIC_Type;
    This topic has been closed for replies.

    4 replies

    Kang Sung Gu
    Associate II
    September 15, 2017
    Posted on September 15, 2017 at 15:24

    Thank you so much

    Tesla DeLorean
    Guru
    September 15, 2017
    Posted on September 15, 2017 at 16:22

    IP[x] where x is the interrupt number (0-239, as implemented)

    and ISER[x / 32] & (1 << (x % 32)) for bit level

    The Data Sheet contains the interrupt numbers as I recall, and the enumeration is also in one of the include files.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    Kang Sung Gu
    Associate II
    September 22, 2017
    Posted on September 22, 2017 at 12:59

    Thank you Clive One