Skip to main content
kishan patel
Associate
September 19, 2017
Question

How can use STM32F429 Discovery Kit?

  • September 19, 2017
  • 3 replies
  • 1007 views
Posted on September 19, 2017 at 09:01

I am new user of stm32f429 discovery kit(STM32F429ZIT6).I have some querry as below:

1).Which software/IDE should i use for programming?.

2).Any sample code to interface OV9655 camera with this kit?

3). How should i interface it?

4).Any sdk for programming?.

Please guide me if possible step by step.

#stm32f4-d
This topic has been closed for replies.

3 replies

ST Technical Moderator
September 28, 2017
Posted on September 28, 2017 at 16:34

Hello,

Have a look at the STM32F4 examples and these include code to run the OV9655 camera and follow the instruction in the readme.txt file:

  •  SPL: STM32F4xx_DSP_StdPeriph_Lib_V1.8.0\Project\STM32F4xx_StdPeriph_Examples\DCMI\DCMI_CameraExample

or

  • Cube: STM32Cube_FW_F4_V1.16.0\Projects\STM324x9I_EVAL\Examples\DCMI

Refer to this 

http://www.st.com/content/ccc/resource/technical/document/application_note/group0/c0/ef/15/38/d1/d6/49/88/DM00373474/files/DM00373474.pdf/jcr:content/translations/en.DM00373474.pdf

Application note 'Digital camera interface (DCMI) for STM32 MCUs' with more description and details about the 

OV9655

camera type used in that board.

Best Regards

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
Tesla DeLorean
Guru
September 28, 2017
Posted on September 28, 2017 at 16:48

Keil works very well.

The STM32F429-DISCO is a very pin limited platform, most committed to SDRAM and LCD, I'd be surprised if the DCMI interface can be exported. Look at the EVAL boards, or third-part boards.

The HAL and SPL have assorted examples, but not for your specific board, you'll have to review and decide if you have the skill set to port them.

Professional guidance is expensive, Google for tutorials or blogs if you need detail for rote implementation.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
kishan patel
Associate
September 29, 2017
Posted on September 29, 2017 at 08:06

Thanks for reply,

Currently,I have interface ov2640 camera with my board.I got

firmware resource from

https://www.waveshare.com/wiki/File:OV2640-Camera-Board-Code.7z link.

I can read the camera product id,also got DCMI-interrupt.But i could not

get DMA-interrupt.So,what should be wrong.

Can you tell me the proper interface pins with camera.

I has refer AN5020 as you told.Now i have confusion that is my

stm-board support camera or not.Please clarify me.

Board: STM32F429 Discovery kit (STM32F429ZIT6).

I am waiting,

Thanks & Regards,

Kishan Patel.

On Thu, Sep 28, 2017 at 8:19 PM, Clive One <st-microelectronics@jiveon.com>