2018-03-09 7:36 AM
We are trying to establish and send and receive Project through an ethernet connection .we use Nucleo f429ZI,
We have our nucleo with
static ip 10.1.1.2 mask 255.255.255.0 gateway 10.1.1.1 using cubemx ,PHY 0,
pc is used az destination having adress 10.1.1.3 using Hercules application
tcpip like a transport protocol.
i can ping my cart using comand mode no prblm.
-i can send by
/* init code for LWIP */
MX_LWIP_Init();
nc=netconn_new(NETCONN_TCP);//create new network connection TCP TYPE
res=netconn_bind(nc,&local_ip,0); //ASSCOCIATE STM MAC ADRESS TO AN IP.--->10.1.1.2 here 0 means any port number so we can accept any port
res=netconn_connect(nc,&remote_ip,23); //connect to remote ip remote port--->our pc server application wireshark for exmple 139
sprintf(send_buffer,'hello from STM32f429 port 23\n\r');
res=netconn_write(nc,send_buffer,strlen(send_buffer),NETCONN_COPY)
-İ can receive by
netconn_accept(nc,&in_nc);
res=netconn_recv(in_nc,&nb);//nc the network connection from which to receive data, nb network buffer
netbuf_copy(nb,buffer,len);
len=netbuf_len(nb);
printf('Received %d bytes:\r\n %s\r\n',len,buffer);
netbuf_delete(nb);//delete data buffer
buffer[len]=0;
but if i put both of them send and receive my prgm bugs and i dont have any reaction
im using FRTOS default task for the moment .i also tried withous frtos. No improvement and also tried to increase the mem size reserved to the thread no difference.
osThreadDef(defaultTask, StartDefaultTask, osPriorityIdle, 0,256);---Ã 1000
defaultTaskHandle = osThreadCreate(osThread(defaultTask), NULL);
so:
-should i use different ports one for receiving one for sending or i can use one port for both?.
-should i create two connections nc , two bindings one sending one for receiving , or one is enough?
-demos are done in a complex way so that i decided to find a simplest way is there a good example or doc using LWİP /netconn functions ?
-serverdemos Works with both straight and cross cable which one is the right ??
-is Ethernet fullduplex ? is there an option i need to add in cubemx to have data both sides going?
Thanks