Skip to main content
Samuele Savoldelli
Visitor II
September 25, 2017
Question

Porting F7 SDIO+FatFs+FreeRTOS project from MxCube 4.22.0 to 4.22.1

  • September 25, 2017
  • 0 replies
  • 398 views
Posted on September 25, 2017 at 13:56

Hi everyone,

lately I had got some trouble with SDIO + Fatfs + FreeRTOS.

Sometimes f_write did not work and, after 100 (more or less) file write the SDIO halted.

Following this link

https://community.st.com/docs/DOC-1546-cubemx-sdio-dma-fatfs-configuration

I discovered that the solution is to introduce DMA on SDIO and, with this configuration:

STM32Cube FW_F7 V1.7.0

+

FatFS version 0.11

it works!!!

Last week ST released a new update for STMCube, so I migrate my project to the new library:

STM32Cube FW_F7 V1.8.0

+

FatFS version 0.12c

I noticed that in STM32Cube there is a new option 'DMA Template' for FatFs so I think 'wow! now the write DMA is fixed!'

Instead with new FW package all the FatFs instruction for SDIO (like f_mount or f_open) reach the timeout.

I can make a step back and use the older version (STM32Cube FW_F7 V1.7.0) but I want to understand if there is something more to do in order to have SDIO works properly

Thanks in advice,

Samuele
    This topic has been closed for replies.