Skip to main content
NItin Kanani
Associate III
Jan 4, 2018 7:44 AM UTC
Question

LIS2DE12

Posted on January 04, 2018 at 08:44

I am interfacing sensor with Micro controller and controller is working at +3.3V.

VDD_IO and VDD are two power supply pins in sensor.

If i am giving common supply +3.3V of controller to VDD_IO and VDD , will it work?

OR

Do i need to give seperate voltages for both supply pins?

Suggest me.

Thanks.

This topic has been closed for replies.

1 reply

ST Employee
Jan 4, 2018 8:19 AM UTC
Posted on January 04, 2018 at 09:19

Yes, it will work. You can tie VDD_IO and VDD together and connect both to 3.3V.