Skip to main content
prateek agrawal
Associate II
Oct 4, 2017 5:38 AM UTC
Question

spi2 not working in stm32f070

Posted on October 04, 2017 at 07:38

Hello All

currently i am working in Fatfs with stm32f070 with spi1.

when i move to spi2 its not working.

i am trying multiple times but i cant get success.

here is my init function

void SPIFlashInit(void)

{

SPI_InitTypeDef SPI_Struct;

GPIO_InitTypeDef GPIO_Struct;

uint32_t stat;

RCC_APB1PeriphClockCmd(RCC_APB1Periph_SPI2, ENABLE);

RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOB ,ENABLE);

RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA ,ENABLE);

GPIO_Struct.GPIO_Pin = GPIO_Pin_15;

GPIO_Struct.GPIO_Mode = GPIO_Mode_OUT;

GPIO_Struct.GPIO_Speed = GPIO_Speed_50MHz;

GPIO_Init(GPIOA, &GPIO_Struct);

GPIO_WriteBit(GPIOA,GPIO_Pin_15,Bit_SET);

// Configure SPI1 pins: SCK, MISO and MOSI

GPIO_Struct.GPIO_Pin =

GPIO_Pin_13

|

GPIO_Pin_14

|

GPIO_Pin_15

;

GPIO_Struct.GPIO_Mode = GPIO_Mode_AF;

GPIO_Init(GPIOB, &GPIO_Struct);

//Configure I/O for Flash Chip select //

GPIO_PinAFConfig(GPIOB,GPIO_PinSource13,GPIO_AF_0);

GPIO_PinAFConfig(

GPIOB

,GPIO_PinSource14,GPIO_AF_0);

GPIO_PinAFConfig(

GPIOB

,GPIO_PinSource15,GPIO_AF_0);

//SPI1 configuration

SPI_Struct.SPI_Direction = SPI_Direction_2Lines_FullDuplex;

SPI_Struct.SPI_Mode = SPI_Mode_Master;

SPI_Struct.SPI_DataSize = SPI_DataSize_8b;

SPI_Struct.SPI_CPOL = SPI_CPOL_Low;

SPI_Struct.SPI_CPHA = SPI_CPHA_1Edge;

SPI_Struct.SPI_NSS = SPI_NSS_Soft;

SPI_Struct.SPI_BaudRatePrescaler = SPI_BaudRatePrescaler_2;

SPI_Struct.SPI_FirstBit = SPI_FirstBit_MSB;

SPI_Struct.SPI_CRCPolynomial = 7;

SPI_Init(SPI2, &SPI_Struct);

SPI_RxFIFOThresholdConfig (SPI2,SPI_RxFIFOThreshold_QF);

SPI_Cmd(SPI2, ENABLE);

}

please ans me where i am wrong in this code.

Note: this post was migrated and contained many threaded conversations, some content may be missing.
    This topic has been closed for replies.

    10 replies

    Vangelis Fortounas
    Associate II
    Oct 4, 2017 12:37 PM UTC
    Posted on October 04, 2017 at 14:37

    Hello!

    What is your device exactly?

    0690X00000608NAQAY.png

    As you can see AF0  SPI2 is available on F070xB devices

    Regards.

    vf

    prateek agrawal
    Associate II
    Oct 4, 2017 3:50 PM UTC
    Posted on October 04, 2017 at 15:50

    hi,

    i am using stm32f070 device. i know that its available on AF0  as you can see in my design. i am using AF0 for SPI2.

    in my debug i can see that it will stuck on

    FlagStatus SPI_I2S_GetFlagStatus(SPI_TypeDef* SPIx, uint16_t SPI_I2S_FLAG){}

    for SPI_I2S_FLAG_RXNE: Receive buffer not empty flag.

    Vangelis Fortounas
    Associate II
    Oct 4, 2017 5:45 PM UTC
    Posted on October 04, 2017 at 17:45

    Hello.

    So. .. this is not an SPI initialization problem.

    Did you change also the porting functions concern SPI1 inside user_diskio.c file.?

    Rgrds

    vf