Question
TIMPRE HCLK multiplier in F413
Posted on May 17, 2018 at 11:08
In RM0430 rev 7 section 6.2 it is stated that when TIMPRE is set and APB prescaler is 1 or 2 then the timer clock is HCLK.
And when APB prescaler is > 2 then the timer clocks are HCLK * 4.This is different to the F446 which in RM0390 section 6.2 which states that when APB prescaler is > 4 then timer clocks will be HCLK * 4.So is the F413 indeed different as stated in the RM or is this a typo in the RM and the F413 is the same as the F446?