Skip to main content
Randy Nelson
Associate III
February 16, 2018
Solved

Which register selects the clock input to a STM32F303K8

  • February 16, 2018
  • 7 replies
  • 1232 views
Posted on February 16, 2018 at 19:22

The clock diagram in RM0316 for the 32F303K8 indicates a clock selection mux off the APBx prescalers. I've searched the registers and cannot find the register used to select one of 4 clock inputs. The 4 possible inputs are the LSE, HSI, SYSCLK, or the clock off the APBx prescaler. The outpu tis to the usuart.

Can someone point me to the register. 

Thanks...

Randy

    This topic has been closed for replies.
    Best answer by Randy Nelson
    Posted on February 16, 2018 at 19:46

    Clive,

    Yes this is the register and thanks.

    Randy

    7 replies

    Randy Nelson
    Associate III
    February 16, 2018
    Posted on February 16, 2018 at 19:32

    Sorry missed indicating the whole point. I'm trying to select the input clock for the Usuart1 and/or Usuart(2..5).

    Randy

    Tesla DeLorean
    Guru
    February 16, 2018
    Posted on February 16, 2018 at 19:43

    RCC_CFGR3

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    Tesla DeLorean
    Guru
    February 16, 2018
    Posted on February 16, 2018 at 19:34

    http://www.st.com/content/ccc/resource/technical/document/reference_manual/4a/19/6e/18/9d/92/43/32/DM00043574.pdf/files/DM00043574.pdf/jcr:content/translations/en.DM00043574.pdf

     

    SW bits of RCC_CFGR

    The USART clock typically depend on the specific APB to which they are attached. ie USART1 on APB2 (fast bus), see RCC_APB2ENR

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    Randy Nelson
    Associate III
    February 16, 2018
    Posted on February 16, 2018 at 19:43

    Clive,

    I understand what you are saying but 'Figure 10. Clock tree' indicates the AHB drives both the APB1 and APB2 which gens PCLK1 and PCLK2. There is a 4-to-1 mux that can select as an input to the USUART either PCLK(1or2) or SYSCLK or HSI or LSE.

    The RCC_CFGR->SW only selects:

    00:HSI

    01:HSE

    10:PLL

    11:not allowed

    These signals names do not match. 

    Randy

    Tesla DeLorean
    Guru
    February 16, 2018
    Posted on February 16, 2018 at 19:44

    Sorry took me a while to dig through, and see second post

    For the peripheral level muxing...

    9.4.13 Clock configuration register 3 (RCC_CFGR3)

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..