Skip to main content
Zhang Lei
Associate II
October 26, 2017
Question

How could I read out the hex file from SPC560P34L1CEFA?

  • October 26, 2017
  • 10 replies
  • 2220 views
Posted on October 26, 2017 at 09:07

How could I read out the hex file from SPC560P34L1CEFA?

#hex
    This topic has been closed for replies.

    10 replies

    Erwan YVIN
    ST Technical Moderator
    October 26, 2017
    Posted on October 26, 2017 at 10:10

    Hello Zhang ,

    Yes , it should be ok for an uncensored chip.

    for a censored one , you need the password.

    You should take the hand with a debugger 

    Example : for PLS , there is a Macro SaveHex <file> <range>

    I have never tested this feature.

                Best Regards

                         Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
    Zhang Lei
    Zhang LeiAuthor
    Associate II
    October 27, 2017
    Posted on October 27, 2017 at 03:41

    I got the following information:

    '_______________________________________________________

    '

    '    SaveHEX command line function

    '

    '    generates intel-HEX file

    '

    '    command line SaveHex output-file range1 [range2] [range3] .....

    '    range description:

    '        <startaddress>,<length>

    '_______________________________________________________

    Sub SaveHEX(File,ParameterObj)

        set debugger = workspace.Coredebugger(0)

        set DisASMObj = debugger.DisASMObj

        If Not IsObject(ParameterObj) Then

              MsgBox ''Number of parameters wrong''

            Exit Sub         

        End If

        If IsNumeric(File) Then

              MsgBox ''File parameter wrong - '' & File

            Exit Sub         

        End If

        DisASMObj.OutputPath = CStr(File)

        bRetVal = DisASMObj.CreateStream(True,''UDE generated intel-Hex file of current Program'',False)

        If bRetVal = True Then

            ParmeterCnt = ParameterObj.ParameterCount

            If ParmeterCnt = 0 Then

                  MsgBox ''Number of parameters wrong '' & ParmeterCnt

                Exit Sub         

            End If

            If ( ParmeterCnt Mod 2 ) <> 0 Then

                  MsgBox ''Number of parameters wrong '' & ParmeterCnt

                Exit Sub         

            End If

            RangeCnt = ParmeterCnt/2

            ParamIndex = 0

            For Range = 0 To RangeCnt -1

                Address = CLng(ParameterObj.Parameter(ParamIndex))        

                Length = CLng(ParameterObj.Parameter(ParamIndex +1))

                ParamIndex = ParamIndex +2

                 DisASMObj.AddRange Address,Length,0

            Next

            DisASMObj.HexFileModeFlag = True

            DisASMObj.WriteAllRanges(False)

        End If

    End Sub

    In the following, what should I insert into it? Could I insert something into it like this ''Application.hex 0x0~0x7FFF''?

    0690X00000604AOQAY.jpg
    Tesla DeLorean
    Guru
    October 27, 2017
    Posted on October 27, 2017 at 04:04

    The instructions suggest something more like

    SaveHEX Application.hex 0,0x8000

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    Erwan YVIN
    ST Technical Moderator
    October 27, 2017
    Posted on October 27, 2017 at 10:39

    Hello Zhang ,

    You have to run the script

    there is a button to do that

    and check the Windows directory

          Best regards

                    Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
    Zhang Lei
    Zhang LeiAuthor
    Associate II
    October 27, 2017
    Posted on October 27, 2017 at 10:50

    I use the following buttons and there is no Application.hex in the Windows directory.

    0690X00000604AnQAI.jpg0690X00000604AsQAI.jpg
    Erwan YVIN
    ST Technical Moderator
    October 27, 2017
    Posted on October 27, 2017 at 14:01

    Hello Zhang ,

    No , You should run the macro script not the embedded software.

             Best regards

                                Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.