Question
Power consumption issue with STM32L073VBT6.
Posted on October 28, 2017 at 12:45
I have my own product board with STM32L073VBT6.The power comsumption increase to 10mA (an other is 4mA) when enter low power mode.So I had removed all other chips only left the STM32 and found out that the MCU cost the 10mA. The function of the chip is ok. I Don't understand How the chip came to that with the function ok.
?????STM32L073??pCB????????10mA??????????????IC??????????3?mA????????????????????????
#stm32l073 #low-power-run #issue