Skip to main content
ren yong
Associate II
October 28, 2017
Question

Power consumption issue with STM32L073VBT6.

  • October 28, 2017
  • 2 replies
  • 644 views
Posted on October 28, 2017 at 12:45

 I have my own product board with STM32L073VBT6.The power comsumption increase to 10mA (an other is 4mA) when enter low power mode.So I had removed all other chips only left the STM32 and found out that the MCU cost the 10mA. The function of the chip is ok. I Don't understand How the chip came to that with the function ok.

?????STM32L073??pCB????????10mA??????????????IC??????????3?mA????????????????????????

#stm32l073 #low-power-run #issue
This topic has been closed for replies.

2 replies

Tesla DeLorean
Guru
October 28, 2017
Posted on October 28, 2017 at 16:47

Unfortunately your post lacks sufficient detail to replicate or understand the circuit and software as implemented.

Is this with a debugger attached?

How to you make a determination about the internal state of the processor?

Sleep/Standby?

External buffers, LEDs, pull up/down resistors?

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
ren yong
ren yongAuthor
Associate II
November 8, 2017
Posted on November 08, 2017 at 02:27

         Just power on with 3.3 the mcu,and connect the reset pin to gnd.