Skip to main content
kurt dewulf
Associate
March 15, 2018
Question

STM32L071KBUx UFQFPN32 exposed pad

Posted on March 15, 2018 at 12:13

I'm drawing a new design with the STM32L071KBUx #UFQFPN32. 

Do I have to connect the exposed pad to the GND, or can I leave it open. I don't see any note in the datasheet DM00141136.pdf, so I think that I can leave it open ?

    This topic has been closed for replies.

    3 replies

    T J
    Senior III
    March 15, 2018
    Posted on March 15, 2018 at 23:58

    connected to ground usually, can you use a meter to check it ?

    the smaller QFN style chip has the rating like 36degrees raise in temp at 1W...

    these stm32L parts are supposed to be low power,

    at 32MHz I cant see then getting warm.

    do you have one running ?, does it get hot ?

    kurt dewulf
    Associate
    March 16, 2018
    Posted on March 16, 2018 at 07:40

    I don't have the device yet (proto phase).

    T J
    Senior III
    March 16, 2018
    Posted on March 16, 2018 at 08:04

    It’s not mentioned in the data sheet, so don’t connect it.

    I would be surprised if the chip gets warm under load,

    You would have to make that assessment when you have it running.

    Otherwise on the PCB, just send a couple of via’s through and heat sink it.. a bit.