How to set the max buffer size for DMA in STM32L4?
- November 21, 2017
- 8 replies
- 2657 views
I am trying to collect data using ADC + DMA continuous mode. I aim to get 2400 data points using DMA. The code is based on the one generated using STM32CubeMx. The data I got from my PC using UART were just 2048 points. I guess I need to change the max buffer size of the DMA. I try to set the CNDTR register in the initialization, but it was not successful. I guess the location could be wrong, or there are other codes required.
I am new to the STM32 family. I hope someone can help me address it. I also attached all my codes.
// partial codes.
//This is the function in main.c.
HAL_ADC_Start_DMA(&hadc1,(uint32_t*)adcValue,2400);
//DMA initialization (Partial)
:
void HAL_ADC_MspInit(ADC_HandleTypeDef* hadc)
{/* ADC1 DMA Init */
/* ADC1 Init */ hdma_adc1.Instance = DMA1_Channel1; hdma_adc1.Init.Request = DMA_REQUEST_0; hdma_adc1.Init.Direction = DMA_PERIPH_TO_MEMORY; hdma_adc1.Init.PeriphInc = DMA_PINC_DISABLE; hdma_adc1.Init.MemInc = DMA_MINC_ENABLE; hdma_adc1.Init.PeriphDataAlignment = DMA_PDATAALIGN_BYTE; hdma_adc1.Init.MemDataAlignment = DMA_MDATAALIGN_BYTE; hdma_adc1.Init.Mode = DMA_CIRCULAR; hdma_adc1.Init.Priority = DMA_PRIORITY_LOW; hdma_adc1.Instance->CNDTR = DataLength; // I was trying to change the buffer size here, but it did work. if (HAL_DMA_Init(&hdma_adc1) != HAL_OK) { _Error_Handler(__FILE__, __LINE__); }__HAL_LINKDMA(hadc,DMA_Handle,hdma_adc1);
}
Thanks in advance.
Hailing
#buffer-size #stm32l4-hal #dma-stm32