Skip to main content
G S
Associate II
November 15, 2017
Solved

what's wrong with my ADC DMA initialization?

  • November 15, 2017
  • 7 replies
  • 1587 views
Posted on November 15, 2017 at 22:13

Hello,

I'm trying to trigger an ADC conversion externally from TRGO2 and store it to a buffer through DMA. However, it doesn't appear that anything is being written to that buffer. Could someone please look through my initialization code and let me know if I'm messing something up during the initialization?

void InitADC(void)
{
int i;
ADC_InitTypeDef ADC_InitStructure;
ADC_CommonInitTypeDef ADC_CommonInitStructure;
GPIO_InitTypeDef GPIO_InitStructure;
NVIC_InitTypeDef NVIC_InitStructure;
DMA_InitTypeDef DMA_InitStructure;

RCC_AHBPeriphClockCmd(RCC_AHBPeriph_DMA1, ENABLE);
DMA_DeInit(DMA1_Channel1);
DMA_InitStructure.DMA_BufferSize = 2;
DMA_InitStructure.DMA_DIR = DMA_DIR_PeripheralSRC;
DMA_InitStructure.DMA_M2M = DMA_M2M_Disable;
DMA_InitStructure.DMA_MemoryBaseAddr = (uint32_t)adcBuffer;
DMA_InitStructure.DMA_MemoryDataSize = DMA_MemoryDataSize_HalfWord;
DMA_InitStructure.DMA_MemoryInc = DMA_MemoryInc_Enable;
DMA_InitStructure.DMA_Mode = DMA_Mode_Circular;
DMA_InitStructure.DMA_PeripheralBaseAddr = (uint32_t)&ADC2->DR;
DMA_InitStructure.DMA_PeripheralDataSize = DMA_PeripheralDataSize_HalfWord;
DMA_InitStructure.DMA_PeripheralInc = DMA_PeripheralInc_Disable;
DMA_InitStructure.DMA_Priority = DMA_Priority_High;
DMA_Init(DMA1_Channel1, &DMA_InitStructure);
DMA_Cmd(DMA1_Channel1, ENABLE);
/* Configure the ADC clock */
RCC_ADCCLKConfig(RCC_ADC12PLLCLK_Div2);
/* Enable ADC12 clock */
RCC_AHBPeriphClockCmd(RCC_AHBPeriph_ADC12, ENABLE);
ADC_CommonInitStructure.ADC_Mode = ADC_Mode_Independent;
ADC_CommonInitStructure.ADC_Clock = ADC_Clock_SynClkModeDiv1;
ADC_CommonInitStructure.ADC_DMAAccessMode = ADC_DMAAccessMode_1;
ADC_CommonInitStructure.ADC_DMAMode = ADC_DMAMode_OneShot;
ADC_CommonInitStructure.ADC_TwoSamplingDelay = 0;
ADC_CommonInit(ADC2, &ADC_CommonInitStructure);
/* GPIOA Periph clock enable */
RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA, ENABLE);
/* Configure ADC2 Channel1 as analog input */
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_4 | GPIO_Pin_5;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AN;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL ;
GPIO_Init(GPIOA, &GPIO_InitStructure);
ADC_StructInit(&ADC_InitStructure);
/* Calibration procedure */
ADC_VoltageRegulatorCmd(ADC2, ENABLE);
for(i = 0; i < 1000; i++) {}
ADC_SelectCalibrationMode(ADC2, ADC_CalibrationMode_Single);
ADC_StartCalibration(ADC2);
while(ADC_GetCalibrationStatus(ADC2) != RESET );
ADC_InitStructure.ADC_ContinuousConvMode = ADC_ContinuousConvMode_Disable;
ADC_InitStructure.ADC_Resolution = ADC_Resolution_12b;
ADC_InitStructure.ADC_ExternalTrigConvEvent = ADC_ExternalTrigConvEvent_10;
ADC_InitStructure.ADC_ExternalTrigEventEdge = ADC_ExternalTrigEventEdge_RisingEdge;
ADC_InitStructure.ADC_DataAlign = ADC_DataAlign_Right;
ADC_InitStructure.ADC_OverrunMode = ADC_OverrunMode_Disable;
ADC_InitStructure.ADC_AutoInjMode = ADC_AutoInjec_Disable;
ADC_InitStructure.ADC_NbrOfRegChannel = 2;
ADC_Init(ADC2, &ADC_InitStructure);
/* ADC2 regular channel1 configuration */
ADC_RegularChannelConfig(ADC2, ADC_Channel_1, 1, ADC_SampleTime_7Cycles5);
ADC_RegularChannelConfig(ADC2, ADC_Channel_2, 2, ADC_SampleTime_7Cycles5);
#warning 'Figure out priority'
/* Configure and enable ADC2 interrupt */
NVIC_InitStructure.NVIC_IRQChannel = ADC1_2_IRQn;
NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0;
NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0;
NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;
NVIC_Init(&NVIC_InitStructure);
/* Enable EOS interrupt */
ADC_ITConfig(ADC2, ADC_IT_EOS, ENABLE);
/* Enable ADC2 */
ADC_Cmd(ADC2, ENABLE);
ADC_DMACmd(ADC2, ENABLE);
/* wait for ADRDY */
while(!ADC_GetFlagStatus(ADC2, ADC_FLAG_RDY));
/* Start ADC2 Software Conversion */
ADC_StartConversion(ADC2);
}
void ADC1_2_IRQHandler(void)
{
 if(ADC_GetFlagStatus(ADC2, ADC_FLAG_EOS) != RESET)
 {
 /* Clear ADC2 AWD pending interrupt bit */
 ADC_ClearITPendingBit(ADC2, ADC_IT_EOS);
adcBuffer[0] = (adcBuffer[0] * ADC_VREF) >> 12;
adcBuffer[1] = (adcBuffer[1] * ADC_VREF) >> 12;
 }
}�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?

Question 2: The schematic I'm working with is using ADC peripheral 1 and ADC peripheral 2 as part of the group of signals I'd like to sample during the TRGO2 event. Do I need to set up a different DMA channel to capture the sample from the other peripheral?

Thanks.

#dma-adc #dma-transfer #stm32f3
This topic has been closed for replies.
Best answer by G S
Posted on November 17, 2017 at 21:17

I appear to have solved the issue. Looking further in the datasheet I realized that ADC2 was not connected to DMA1 channel 1

0690X0000060PFOQA2.png

The correct DMA connection to ADC2 is DMA2 Channel 1:

0690X0000060PFPQA2.png

7 replies

waclawek.jan
Super User
November 15, 2017
Posted on November 16, 2017 at 00:46

Which mcu?

Did you verify that your trigger source works and the trigger is set properly in timer?

JW

G S
G SAuthor
Associate II
November 16, 2017
Posted on November 16, 2017 at 06:21

Yes, trigger source works. The ADC interrupt is firing and I can read the value directly from there, however the adcBuffer which is the address the DMA is set to is empty.

I'm using the STM32F303VC. 

waclawek.jan
Super User
November 16, 2017
Posted on November 16, 2017 at 09:41

Remove (don't enable) the interrupt. Instead, use the transfer complete interrupt from DMA.

Make sure both DMACFG and DMAEN are set in ADCx_CFGR.

JW

G S
G SAuthorBest answer
Associate II
November 17, 2017
Posted on November 17, 2017 at 21:17

I appear to have solved the issue. Looking further in the datasheet I realized that ADC2 was not connected to DMA1 channel 1

0690X0000060PFOQA2.png

The correct DMA connection to ADC2 is DMA2 Channel 1:

0690X0000060PFPQA2.png