Associate II
November 21, 2017
Solved
Regarding ADC input source on STM32F3Discovery board
- November 21, 2017
- 14 replies
- 19743 views
Posted on November 21, 2017 at 13:27
Dear All,
I'd like to test an ADC conversion using ADC example from STM32F3Discovery's peripheral examples.
I connected ADC1 channel(PC1) and GND to external power supply directly. and It was measured anormalvoltage between PC1 and GND using FLUKE Multimeter 8846A.
But, as attached the ADC value on Terminal I/O, theresults are very unstable. Is that due to the bad connection for ADC input source? or I cannot catch the problem exactly. Could you please help the issue?
1. supplying 0V to ADC1 channel(PC1)
2. supplying 1.0V to ADC1 channel(PC1)