Skip to main content
Emre Ozkan
Visitor II
November 21, 2017
Question

Using X-CCA02M1 board,How can I get the accuracy in AcousticSL two mic. configuration ?

  • November 21, 2017
  • 0 replies
  • 534 views
Posted on November 21, 2017 at 19:08

Hi everyone,

I am using Nucleo f401-Re board with X-Nucleo-CCA02M1 board. I am experiencing with the sample Acoustic Sound Location code. I successfully uploaded and experienced with 4 microphone configuration. Now I am trying to work with 2 channel in 180 degree configuration. However, the angles are not accurate as much as 4 microphone configuration. Is there any suggestion about it? I changed the channel number in here : libSoundSourceLoc_Handler_Instance.channel_number = 2;    and also here :  libSoundSourceLoc_Handler_Instance.ptr_M1_channels = 2;

libSoundSourceLoc_Handler_Instance.ptr_M2_channels = 2;

libSoundSourceLoc_Handler_Instance.ptr_M3_channels = 2;

libSoundSourceLoc_Handler_Instance.ptr_M4_channels = 2;

If I choose 0 for M3 and M4 channels the system does not give any angles so I am working with these configuration but the angles are not accurate. 

Looking forward to hearing something from you guys.

Thank you in advance,

#x-cca02m1-acousticsl-two-mic-configuration-180-degree #x-nucleo-cca02m1 #acousticsl #stm32
This topic has been closed for replies.