Skip to main content
guo sir
Associate
November 26, 2017
Question

About stm32L stop mode uart

  • November 26, 2017
  • 1 reply
  • 574 views
Posted on November 26, 2017 at 13:58

hi everyone~

Before  enter stop mode ,I called HAL_UART_DeInit(&huart3) an  after it was  wake up from stop mode(wake up by rtc), I called HAL_UART_Init(&huart3),but after wake up uart3 can't work. What should I do?

before enter stop mode:

  huart3.Instance = USART3;

  if (HAL_UART_DeInit(&huart3) != HAL_OK)

  {

    _Error_Handler(__FILE__, __LINE__);

  }

wake up from stop mode:

  huart3.Instance = USART3;

  huart3.Init.BaudRate = 9600;

  huart3.Init.WordLength = UART_WORDLENGTH_8B;

  huart3.Init.StopBits = UART_STOPBITS_1;

  huart3.Init.Parity = UART_PARITY_NONE;

  huart3.Init.Mode = UART_MODE_TX_RX;

  huart3.Init.HwFlowCtl = UART_HWCONTROL_NONE;

  huart3.Init.OverSampling = UART_OVERSAMPLING_16;

  if (HAL_UART_Init(&huart3) != HAL_OK)

  {

    _Error_Handler(__FILE__, __LINE__);

  }
    This topic has been closed for replies.

    1 reply

    Tesla DeLorean
    Guru
    November 26, 2017
    Posted on November 26, 2017 at 17:21

    Look at peripheral view in debugger, make sure no error status in USART which needs clearing. Code robustly so you can identify and clear errors.

    Make sure _Error_Handler() and other potential paths of silent death output blinking LED or GPIO, or output via USART as available, so you know what might be happening when debugger not usable. Output from Hard Fault Handler also strongly recommended.

    Exits from sleep mode may be with different clocks.

    STM32L1 family?

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..