Skip to main content
kiran kanchi
Associate III
December 11, 2017
Question

FCU001V1

  • December 11, 2017
  • 9 replies
  • 4424 views
Posted on December 11, 2017 at 18:55

I bought the fcu001v1, the device just started to blink of led LD2 and LD1 off, i tried searching for bluetooth connectivity. device was not listed.

i tried to connect the SWD of FCU001V1 through my STlink V2 on STM32F4 Discovery, but device is not detected.

does the micro usb port configured as USB device for DFU firmware update ? it is not detected as USB device on my PC.

Please help......

i followed this connection

    This topic has been closed for replies.

    9 replies

    Matteo MARAVITA
    ST Employee
    April 11, 2018
    Posted on April 11, 2018 at 06:57

    Hi Kiran,

    I think we already solved above issue with separate discussion on Github platform.

    Last week we opened a new community specific for Drone, please kindly have a look and if any question post here:

    https://community.st.com/community/drone-zone

    Also it would be very appreciated if you may share with other community users any photo or video of the minidrone you built with the ST FCU.

    Matteo

    kiran kanchi
    Associate III
    April 26, 2018
    Posted on April 26, 2018 at 09:13

    Hello, sorry for delay.

    The drone with dc motors is actually a ripped toy. I still dont have 3d printer. However i have fpv250 drone .

    So i am collecting info to work witg 20A esc with fcu.

    Matteo MARAVITA
    ST Employee
    May 7, 2018
    Posted on May 07, 2018 at 02:08

    Hi,

    in case you have no 3D printer you may purchase some small frame from online stores (like Bangood, ...), like the one here: 

     

    With some hot glue it worked quite well for me.

    kiran kanchi
    Associate III
    May 7, 2018
    Posted on May 07, 2018 at 10:48

    Wow, thank you so much for that suggestion.

    I have already tried with a crappy not so well balanced toy quad frame and

    it didnt work mainly because of Pid Mismatch.

    Anyway with the new frames that you suggested can i use stock pid

    parameters or do you have a well defined set of them ?

    On Mon, 7 May 2018, 5:38 a.m. Matteo Maravita, <