Skip to main content
Zhentao Lu
Associate
April 12, 2018
Question

I got ''Target power failure'' error when I built a project

  • April 12, 2018
  • 17 replies
  • 4269 views
Posted on April 12, 2018 at 04:45

I bought a development board -STM3210C-SK/RAIS [Development Boards & Kits - ARM Raisonance]. I intalled the Ride 7 from the CD in the package, set up and confirmed all jumpers then opened an example - QuickStart_STM32F After I clicked the Project -> Build Project command, there is an error saying that ''Target power failure: Measured 0.000000V.

There is a quick start manual.

0690X00000604ZPQAY.jpg

The error:

0690X00000603leQAA.jpg

In Debug options window, if I clicked

“Connect to Debugger�?, then:

0690X00000604ZTQAY.jpg

I assume that the board has already connected with my computer.

This is my board:

0690X0000060401QAA.jpg

I searched in google and found two websites talking about such error but their boards are not exactly same as my board.

Target power failure: Measured 0.100000V - problem on Windows XP

http://www.stm32circle.com/forum/viewtopic.php?id=86

Topic : I got ''Target power failure'' error when I built a project

http://support.raisonance.com/node/897559

It seems something goes wrong on my board. Does anyone have the same problem? Thank you very much.

Zhentao Lu

#power #stm-32 #failure

Note: this post was migrated and contained many threaded conversations, some content may be missing.
    This topic has been closed for replies.

    17 replies

    AvaTar
    Senior III
    April 12, 2018
    Posted on April 12, 2018 at 07:21

    Raisonance has a forum as well, but they are not mentioned often here.

    Might be worth to register there.

    But to your issue - might it be that the target is really not powered ?

    Not sure if the Raisonance debug pod can power a target, but surely not such a large one as depicted.

    Check the dev board manual for power supply options, and supply it externally.

    Zhentao Lu
    Associate
    April 13, 2018
    Posted on April 13, 2018 at 09:35

    Thank you very much. Actually there is another cable to connect to the daughter board from computer. I didn't connect it in the picture. But it's no help. No matter it is connected or not, there is always such error. I changed to a new cable but it doesn't work. I thought about supplying it externally but I couldn't find a manual in anywhere (CD or paper or website). I'm now thinking to return the board and get money back. Thanks anyway.

    AvaTar
    Senior III
    April 13, 2018
    Posted on April 13, 2018 at 10:14

    I'm pretty sure there are status LEDs on this board, at least for 'power on'.

    And there might jumpers to set, to select a power supply option.

    If ther is no LED at all on, it is suspicious.

    In your place, I would contact Raisonance.

    I know of other companies that hide datasheets and user manuals for their stuff from free access, i.e. one needs a login.

    Andrew Neil
    Super User
    April 13, 2018
    Posted on April 13, 2018 at 10:48

    I bought a development board - STM3210C-SK/RAIS [Development Boards & Kits - ARM

    Raisonance

    ].

    So, if it's a Raisonance board - you should be contacting Raisonance for support! 

    http://www.raisonance.com/raisonance-support.html

     

    http://www.raisonance.com/contact-raisonance.html

     
    A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
    Zhentao Lu
    Associate
    April 13, 2018
    Posted on April 13, 2018 at 11:38

    Thank you very much about the information. I posted my question on Raisonance forum 5 days ago but no one answered. I sent an email to its support email box. Hope it's working. Thanks anyway.

    Andrew Neil
    Super User
    April 13, 2018
    Posted on April 13, 2018 at 13:13

    I haven't used Raisonance for years (in fact, have barely even heard them mentioned) - but their support certainly used to be good ...

    EDIT

    I justtook a look at the 'ARM' section of their website; the picture seems to prominently feature your board:

    http://www.raisonance.com/tzr/scripts/resizer.php?filename=T004/img1/7f/df/4sc72i7ridjx&mime=image%2Fpng&&originalname=tool.png

    So I guess it must be a current product.

    So you should be able to expect good support.

    A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.