Receive UART WWDG_IRQHandler infinite loop
Good morning. I'v tried to perform an UART receive on stm32f407vg board using RXNE interrupt. But when i execute the code it is blocked on WWDG_IRQHandler infinite loop. I post my code:
#include 'stm32f4xx.h'
#include 'stm32f407xx.h'#include 'stm32f4xx_hal_gpio.h'#include 'stm32f4xx_hal_rcc.h'#include 'stm32f4xx_hal.h'#include 'stm32f4xx_hal_uart.h'#include 'stm32f4xx_hal_cortex.h'#include 'stm32f4xx_hal_pwr.h'#include <stdio.h>#include 'semihosting.h'#define UART_BUFFER_SIZE 64
uint8_t UART_BUFFER[UART_BUFFER_SIZE];void HAL_UART_RxCpltCallback(UART_HandleTypeDef *uart_handle) {
int i;
for(i=0; i < UART_BUFFER_SIZE; i++)
printf(uart_handle->pRxBuffPtr[i]);}int main() {
__GPIOA_CLK_ENABLE();
__UART4_CLK_ENABLE(); __PWR_CLK_ENABLE(); __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);RCC_OscInitTypeDef RCC_OscInitStruct;
RCC_ClkInitTypeDef RCC_ClkInitStruct;RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
RCC_OscInitStruct.HSIState = RCC_HSI_ON; RCC_OscInitStruct.HSICalibrationValue = 16; RCC_OscInitStruct.PLL.PLLState = RCC_PLL_NONE;HAL_RCC_OscConfig(&RCC_OscInitStruct);
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
|RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2; RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_HSI; RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1; RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1; RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_0);
HAL_SYSTICK_Config(HAL_RCC_GetHCLKFreq()/1000);
HAL_NVIC_SetPriority(SysTick_IRQn, 0, 0);
GPIO_InitTypeDef gpio_init;
gpio_init.Pin=GPIO_PIN_1;
gpio_init.Mode=GPIO_MODE_AF_PP; gpio_init.Pull=GPIO_PULLUP; gpio_init.Speed=GPIO_SPEED_MEDIUM; gpio_init.Alternate=GPIO_AF8_UART4;HAL_GPIO_Init(GPIOA, &gpio_init);
UART_InitTypeDef uart_init;
uart_init.BaudRate=9600;
uart_init.HwFlowCtl=UART_HWCONTROL_NONE; uart_init.Mode=UART_MODE_RX; uart_init.OverSampling=UART_OVERSAMPLING_16; uart_init.Parity=UART_PARITY_NONE; uart_init.StopBits=UART_STOPBITS_1; uart_init.WordLength=UART_WORDLENGTH_8B;UART_HandleTypeDef uart_handle;
uart_handle.Init=uart_init;
uart_handle.Instance=UART4; uart_handle.RxXferCount=0; uart_handle.RxXferSize=UART_BUFFER_SIZE; uart_handle.pRxBuffPtr=UART_BUFFER;HAL_UART_Init(&uart_handle);
HAL_NVIC_EnableIRQ(UART4_IRQn);
HAL_NVIC_SetPriority(UART4_IRQn, 0, 0);__HAL_UART_ENABLE_IT(&uart_handle, UART_IT_RXNE);
__HAL_UART_ENABLE(&uart_handle);while(1) {
if(__HAL_UART_GET_IT_SOURCE(&uart_handle, UART_IT_RXNE) && __HAL_UART_GET_FLAG(&uart_handle, UART_FLAG_RXNE)) {
HAL_UART_IRQHandler(&uart_handle); }}}
Can you tell me if there is anything wrong? Suggests? Answers? Thank you very much. Goodbye.